0000649744_02_en

Virtual LED Bar

From the message list, a customized selection of indications and alarms will be visible as LEDs in the virtual LED bar. It is also possible to customize if any LED should be held until they are manually reset.

A Hold alarm LED will flash after the active alarm condition is no longer present. It will continue to flash until is it manually reset. When a Hold alarm LED flashes the Reset held alarms button is shown above the LED test button.

Press the Double arrow icon to expand the list and view the names. If there are more LEDs defined than can fit on one screen it is also possible to scroll in the list of LEDs.

It is not recommended to define more LEDs that can fit on the screen as the LEDs have a fix position.

NOTE: An example virtual LED bar is shown. Customized systems might have different LED alarms.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?