VIGED310023FR-06

Conformité aux normes chinoises

Ce produit est conforme aux normes chinoises suivantes :

BS/ EN/ IEC 61557-8 Electrical safety in low voltage distribution systems up to 1 000 V a.c. and 1 500 V d.c. - Equipment for testing, measuring or monitoring of protective measures - Part 8: Insulation monitoring devices for IT systems

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Contenu utile ?