DOCA0162EN-02

Prerequisites

The prerequisites for configuring MasterPacT MTZ IED in IEC 61850 communication standard are:

  • Install the CET850 configuration software in order to create the CID file.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.