DOCA0162EN-02

Introduction

The configuration of MasterPacT MTZ IED includes two operations:

  • MasterPacT MTZ CID.exi file generation (offline configuration) using the CET850 configuration software.

    The CID.exi file can be configured and created offline without any connection to the IFE interface, EIFE interface, or IFE server.

  • CID.exi file transfer to IFE interface, EIFE interface, or IFE server (on-site configuration)

    After the CID.exi file is transferred, it is validated by the IFE interface, EIFE interface, or IFE server.

    • The CID file is transferred to the IFE or EIFE interface with firmware version ≤ V004.005.000 via the FTP protocol using the CET850 configuration software. Refer to the file transfer procedure.

    • The CID file is transferred to the IFE or EIFE interface with firmware version ≥ V004.006.000 via the FTPS protocol using the FTPS client, such as FileZilla or WinSCP Refer to the file transfer procedure.

    • The CID file is transferred to the IFE server with firmware version ≥ V005.001.000 via the FTPS protocol using the FTPS client, such as FileZilla or WinSCP. Refer to the file transfer procedure.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.