DOCA0162EN-02

Preconfigured Datasets

For MasterPacT MTZ IED, six datasets are preconfigured with predefined data values.

NOTICE
COMMUNICATION LOSS
Do not modify the data values of each preconfigured dataset. If the data values are modified, the resulting CID file will not function on the MasterPacT MTZ IED.
Failure to follow these instructions can result in communication loss.

The CET850 configuration software can be used to view datasets in the CID file.

The ICD file for the MasterPacT MTZ IED is preconfigured with six datasets:

Datasets

Description

Health status

Contains the health information of all logical nodes

Breaker status

Contains XCBR, Ext_GGIO1, and CSWI logical nodes

Protections

Contains PTOC, PTOV, PTUV, PTOF, PTUF, PDOP, PTRC, and PIOC logical nodes

Measurements

Contains MMXU and MHAI logical nodes

Energy

Contains MMTR logical node

GGIO

Contains GGIO logical node

The following figure shows the details of preconfigured datasets:

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.