DOCA0162EN-02

Enable CID.exi File for File Transfer

The IFE interface, EIFE interface, or IFE server accepts CID file with CID.exi format only. Before transferring the CID.exi file to IFE interface, EIFE interface, or IFE server, it is mandatory to enable the CID.exi file.

To enable the CID.exi file, in the CET850 configuration software, in Tools > Properties > Preferences, select Use EXI compression format for CID file from the File Export option.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.