DOCA0162EN-02

Configurable Features of IEC 61850 Standard

The datasets are preconfigured. The configurable IEC 61850 features of the MasterPacT MTZ IED are:

  • Report control blocks

  • Reporting triggers

  • Deadband value

  • Circuit breaker control

To set up client connections and enable reports, refer to the CET850 IEC 61850 Configuration Software - User's Manual.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.