DOCA0162EN-02

Conformance Statements (Edition 2.0)

This appendix describes the conformity with IEC 61850 edition 2.0 communication standard. It does not describe the standard itself, only the details of the IEC 61850 implementation of the standard in MasterPacT MTZ IED in terms of services, modeling, exceptions, extensions, and adaptations are described.

The conformance is described in the following statements:

  • Abstract Communication Services Interface (ACSI) conformance statement: Describes the abstract communication services interface (which services are implemented). These services are mapped to Specific Communication Services Model (SCSM) described in the Protocol Implementation Conformance Statement (PICS).

  • Model Implementation Conformance Statement (MICS): Describes how the information model is implemented.

  • Protocol Implementation Conformance Statement (PICS): Describes how the IEC 61850 standard is implemented.

  • Protocol Implementation eXtra Information for Testing (PIXIT): Describes additional implementation-specific information not contained within the previous standard statements.

  • TISSUES Implementation Conformance Statement (TICS): Describes technical issues that have been incorporated into our implementation of the IEC 61850 standard.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.