DOCA0162EN-02

Features

The following table lists the configurable features in the MasterPacT MTZ implementation of IEC 61850 communication standard:

Feature

Description

Datasets

A Dataset (DS) is a collection of data values from any logical node. A maximum of six datasets are preconfigured in .ICD file.

Report Control Blocks

Report Control Blocks (RCBs) are associated with a specific dataset. When the report is enabled and the trigger conditions are met, the report is sent to a specific client. The RCBs are preconfigured.

For more information, refer to Reports Configuration.

Trigger options

The trigger options are specified in the RCB options in the CID file, which includes:

  • Quality change

  • Data change (using deadband values)

  • Data update

  • Integrity period

  • General interrogation

For more information, refer to Reporting Triggers Configuration.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.