DOCA0162EN-02

GGIO Logical Nodes

The GGIO logical nodes supported in the MasterPacT MTZ implementation of IEC 61850 communication standard are:

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.