DOCA0162EN-02

Circuit Breaker Control Configuration

The MasterPacT MTZ IED supports the following control features:

  • Direct control with normal security

  • Select Before Operate (SBO) with normal security

  • Select Before Operate (SBO) with enhanced security (default setting)

NOTE: For circuit breaker operation, the MasterPacT MTZ IED should be Auto: Remote mode to allow control over IEC 61850 communication standard.

To change the control modes use the system engineering tools (for example, PASIC-GEA).

For more information on control model, refer to Control Model.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.