DOCA0162EN-02

About the Book

Document Scope

The objective of this document is to provide users, installers, and maintenance personnel with the technical information required to operate the IEC 61850 communication standard on the following ranges of circuit breakers:

  • MasterPacT™ MTZ1 circuit breakers from 630 to 1600 A with MicroLogic X control unit

  • MasterPacT™ MTZ2 circuit breakers from 800 to 4000 A with MicroLogic X control unit

  • MasterPacT™ MTZ3 circuit breakers from 4000 to 6300 A with MicroLogic X control unit

Validity Note

This document is valid for:

  • MasterPacT MTZ1/MTZ2/MTZ3 circuit breakers.

  • MicroLogic™ X control unit with IEC 61850 for MasterPacT MTZ Digital Module installed

  • Connected to Ethernet network using:

    • An IFE Ethernet interface for one circuit breaker

    • An EIFE embedded Ethernet interface for one MasterPacT MTZ drawout circuit breaker

    • An IFE Ethernet switchboard server, with the MasterPacT MTZ circuit breaker connected to an ULP port of the IFE server.

NOTE: IEC 61850 is not applicable for serial devices.

This document is valid for the devices with a firmware version equal to or greater than the minimum firmware version required:

IMU module

Part number

Firmware version

MicroLogic X control unit

-

≥ V004.000.000

IO module

LV434063

≥ V003.004.005

IFE Ethernet interface

LV434001

≥ V004.001.000

EIFE Ethernet interface

LV851001

≥ V004.001.000

IFE Ethernet server

LV434002

≥ V005.001.000

Use the latest version of EcoStruxure Power Commission (EPC) software to update the device with the latest firmware version available.

Online Information

The information contained in this guide is likely to be updated at any time. Schneider Electric strongly recommends that you have the most recent and up-to-date version available on www.se.com/ww/en/download.

The technical characteristics of the devices described in this guide also appear online. To access the information online, go to the Schneider Electric Country website at www.se.com.

Related Documents for IEC Devices

Title of documentation

Reference number

CET850 IEC 61850 Configuration Software - User's Manual

SEPED306025EN

MasterPacT MTZ MicroLogic X Control Unit - User Guide

ULP (Universal Logic Plug) System for ComPacT and MasterPacT Circuit Breakers - User Guide

Enerlin’X IFE - Ethernet Interface for One Circuit Breaker - User Guide

Enerlin’X EIFE - Embedded Ethernet Interface for One MasterPacT MTZ Drawout Circuit Breaker - User Guide

Enerlin’X - IFE Ethernet Switchboard Server - User Guide

Enerlin’X IO - Input/Output Application Module for One Circuit Breaker - User Guide

You can download these technical publications and other technical information from our website at https://www.se.com/en/download.

Related Documents for UL Devices

Title of documentation

Reference number

CET850 IEC 61850 Configuration Software - User's Manual

SEPED306025EN

MasterPacT MTZ MicroLogic X Control Unit - User Guide

ULP (Universal Logic Plug) System for PowerPacT and MasterPacT Circuit Breakers - User Guide

Enerlin’X IFE - Ethernet Interface for One Circuit Breaker - User Guide

Enerlin’X EIFE - Embedded Ethernet Interface for One MasterPacT MTZ Drawout Circuit Breaker - User Guide

Enerlin’X - IFE Ethernet Switchboard Server - User Guide

Enerlin’X IO - Input/Output Application Module for One Circuit Breaker - User Guide

You can download these technical publications and other technical information from our website at https://www.se.com/en/download.

Information on Non-Inclusive or Insensitive Terminology

As a responsible, inclusive company, Schneider Electric is constantly updating its communications and products that contain non-inclusive or insensitive terminology. However, despite these efforts, our content may still contain terms that are deemed inappropriate by some customers.

Trademark Notice

All trademarks are owned by Schneider Electric Industries SAS or its affiliated companies.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.