DOCA0162EN-02

Address

Address parameters are set to connect the IED to the communication network. Connecting the IED can be done at this stage or later using the Add > Connected Access Point menu.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.