DOCA0162EN-02

Reports Configuration

The CET850 configuration software can be used to view unbuffered reports. Each client connection can enable this report when it is available. This report is sent to the clients who have enabled this report.

This report must be located in LLN0 as it contains data from other logical nodes within that logical device.

NOTE: It is recommended not to modify these data as all the reports are preconfigured.

When unbuffered reports are enabled, the reports are transmitted. If the client is not connected or if there is a communication issue, the report is lost.

NOTICE
LOSS OF DATA
Do not create, modify, or delete preconfigured reports.
Failure to follow these instructions can result in loss of communication or data reports.

The MasterPacT MTZ configuration file is limited to 24 unbuffered reports. This corresponds to a maximum of four client connections with six unbuffered reports for each connection.

NOTE:
  • If the maximum number of reports or client connections exceeds the limit, the IFE interface, EIFE interface, or IFE server will reject the reports for new clients.

  • The minimum refreshment rate of IEC 61850 data is 1 s. The associated MasterPacT MTZ IED data is updated more frequently.

The ICD file for the MasterPacT MTZ IED is preconfigured with six unbuffered reports:

Report

Description

Health status

Reports data from the health status dataset

Breaker status

Reports data from the breaker status dataset

Protections

Reports data from the protections dataset

Measurements

Reports data from the measurements dataset

Energy

Reports data from the energy dataset

GGIO

Reports data from the GGIO dataset

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.