DOCA0162EN-02

TISSUES Implementation Conformance Statement

Introduction

The TISSUES Implementation Conformance Statement (TICS) is required by UCA IUG QAP to perform conformance test.

The supported features are indicated as follows:

  • Y: Implemented

  • Na: Not applicable

Mandatory Interoperability (Intop) Issues

Implemented Intop TISSUES

Part

TISSUE

Description

Implemented

8-1

116

GetNameList with empty response?

Y

165

Improper error response for GetDataSetValues

Y

183

GetNameList error handling

Y

7-4

None

7-3

28

Definition of APC

Na

54

Point def xVal, not cVal

Na

55

Ineut = Ires?

Na

60

Services missing in tables

Na

63

mag in CDC CMV

Y

65

Deadband calculation of a vector and trigger option

Na

219

operTm in ACT

Na

270

WYE and DEL RMS values

Na

7-2

30

Control parameter T

Y

31

Typo

Na

32

Typo in syntax

Na

35

Typo syntax control time

Na

36

Syntax parameter Dset-Ref missing

Na

37

Syntax GOOSE “T” type

Na

39

Add DstAddr to GoCB

Na

40

GOOSE Message AppID to GoID

Na

41

GsCb AppIE to GoID

Na

42

SV timestamp: EntryTime to TimeStamp

Na

43

Control T semantic

Na

44

AddCause - Object not sel

Na

45

Missing AddCauses (neg range)

Na

46

Synchro check cancel

Na

47

“.” in LD name?

Y

49

BRCB TimeOfEntry (part of # 453)

Na

50

LLName start with number?

Y

51

ARRAY [0..num] missing

Y

52

Ambiguity GOOSE SqNum

Na

53

Add DstAddr to GsCB, SV

Na

151

Name constraint for control blocks

Y

166

DataRef attribute in Log

Na

185

Logging - Integrity period

Na

189

SV format

Na

190

BRCB: EntryID and TimeOfEntry (part of #453)

Na

191

BRCB: Integrity and buffering reports (part of #453)

Na

234

New type CtxInt (Enumerated values are mapped to 8 bit integer)

Na

275

Confusing statement on GI usage (part of #453)

Y

278

EntryID not valid for a server (part of #453)

Y

6

1

Syntax

Na

5

ExtensionAttributeNameEnum is restricted

Na

8

SIUnit enumeration for W

Y

10

Base type for bitstring usage

Y

17

DAI/SDI elements syntax

Na

169

Ordering of Enumerated values differs from 7-3

Y

Optional Interoperability (Intop) Issues

Implemented Intop TISSUES

Part

TISSUE

Description

Implemented

8-1

235

Extension of name length

Y

246

Control negative response (SBOns) with LastApplError

Na

545

Skip file directories with no files

Na

7-2

333

Enabling of an incomplete GoCB

Na

453

Combination of all reporting and logging issues

Na

6

245

Attribute RptId in SCL

Y

529

Replace sev - Unknown by unknown

Na

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.