DOCA0162EN-02

TCP/IP Client Connections

The IEC 61850 communication standard is available through the Ethernet port of the IFE interface, EIFE interface, or IFE server, with the MasterPacT MTZ circuit breaker connected to an ULP port of the IFE server. A maximum of four IEC 61850 clients can be connected for each MasterPacT MTZ IED.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.