DOCA0162EN-02

Abstract Communication Services Interface Conformance Statement

The Abstract Communication Services Interface (ACSI) conformance statement is defined by IEC 61850-7-2, and provides the following specifications:

  • A basic information model.

  • Information exchange service models.

The supported features are indicated with an X.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.