DOCA0162EN-02

MasterPacT MTZ CID File Generation (Offline Configuration)

NOTICE
INCOMPATIBLE ICD OR CID FILES
Use only CET850 configuration software to edit ICD or CID files for the MasterPacT MTZ IED.
Failure to follow these instructions can result in configuration discrepancy or communication loss.

For instructions on how to use the CET850 configuration software, refer to the CET850 IEC 61850 Configuration Software - User's Manual.

Step

Action

1

Access the ICD file using the CET850 configuration software.

2

Enter the file properties to configure MasterPacT MTZ IED. The properties that must be configured in the CID file includes:

NOTE: Enter the revision notes and change track information in the header properties.

3

Review the preconfigured datasets and report control blocks.

4

Configure the descriptions (d field) for any logical node leafs if required.

5

Build the CID file.

The following figure shows how to access the ICD file using the CET850 configuration software:



The following figure shows the file properties to be configured in the CID file for MasterPacT MTZ IED:


Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.