DOCA0162EN-02

Supported Models

The supported models are IFE interface, EIFE interface, and IFE server, with the MasterPacT MTZ circuit breaker connected to an ULP port of the IFE server.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.