DOCA0162EN-02

Device Configuration

Adding and removing a device in an IEC 61850 system consists of making the change in the associated SCD file.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.