DOCA0162EN-02

Supported Logical Nodes

The following table lists the logical nodes supported in the MasterPacT MTZ implementation of IEC 61850 communication standard:

Logical Node

Description

CSWI

Switch controller. Used to control circuit breakers.

GGIO

Generic process IO module.

For more information about inputs and outputs of the IO module, refer to Enerlin'X IO - Input/Output Application Module for One Circuit Breaker - User Guide.

LLN0

Logical node zero. Contains the data related to the associated Intelligent Electronic Device (IED).

LPHD

Physical device. Contains information related to the physical device.

MHAI

Harmonics. Consists of harmonic values such as THD.

MMTR

Metering. Consists of the integrated values (energy), primarily for billing purposes.

MMXU

Measurements. Contains per-phase and total current, voltage and power flow for operational purposes.

PTOC

Time overcurrent protection

PIOC

Instantaneous over current protection

PTOV

Over voltage protection

PTUV

Under voltage protection

PDOP

Reverse power protection

PTRC

Protection trip conditioning

XCBR

Circuit breaker. Indicates the status of the circuit breaker.

PTUF

Under frequency protection

PTOF

Over frequency protection

For more information on the logical nodes, refer to Appendix A.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.