DOCA0162EN-02

MasterPacT MTZ IED Definition

The MasterPacT MTZ IED is composed of:

  • One MasterPacT MTZ1, MTZ2, or MTZ3 circuit breaker

  • One MicroLogic X control unit with IEC 61850 for MasterPacT MTZ Digital Module installed

  • One IFE Ethernet interface, EIFE Ethernet interface

    , or IFE Ethernet switchboard server, with the MasterPacT MTZ circuit breaker connected to an ULP port of the IFE server.
  • Optional digital inputs and outputs: one or two IO modules, or one M2C programmable contacts

A MasterPacT MTZ IED can be connected to an IEC 61850 Ethernet network according to Edition 2.0 of the following IEC standards:

  • IEC 61850-6 standard

  • IEC 61850-7-1 to 7-4 standards

  • IEC 61850-8-1 standard

The MasterPacT MTZ IED communication conforms to IEC 61850 standard and Manufacturing Message Specification (MMS) protocol.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.