DOCA0162EN-02

Remove an IED

An IED can be removed from an SCD file. This function is available when an IED is selected in the tree view. After confirming that the IED is to be deleted, the tree view and the content of the SCD file are updated.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.