DOCA0162EN-02

File Transfer Protocol or File Transfer Protocol Secure

For IFE or EIFE interface with firmware version ≤ V004.005.000, use the FTP protocol and CET850 configuration software to transfer the CID.exi files.

For IFE, or EIFE interface with firmware version ≥ V004.006.000, use a FTPS client, such as FileZilla or WinSCP to transfer the CID.exi files.

For IFE server with firmware version ≥ V005.001.000, use a FTPS client, such as FileZilla or WinSCP to transfer the CID.exi files.

The transfer of CID.exi files through FTP or FTPS is password-protected by Role Based Access Control (RBAC) feature in IFE interface, EIFE interface, and IFE server. Only users with Engineer or Installer roles can transfer the CID.exi files.

For more information on user roles, refer to the following user guides in Related Documents:

  • Enerlin’X IFE - Ethernet Interface for One Circuit Breaker - User Guide
  • Enerlin’X EIFE - Embedded Ethernet Interface for One MasterPacT MTZ Drawout Circuit Breaker - User Guide
  • Enerlin’X IFE - Ethernet Switchboard Server- User Guide
  • CET850 IEC 61850 Configuration Software - User's Manual

When a valid CID.exi file has been transferred to the IFE interface, EIFE interface, or IFE server and if the IEC 61850 for MasterPacT MTZ Digital Module is installed in the MicroLogic X control unit. The MasterPacT MTZ IED functions as a server and provides information to the IEC 61850 client substation systems.

The IEC 61850 folders on the IFE interface, EIFE interface, and IFE server are factory-configured and cannot be modified. The file or folder structure of the FTP or FTPS files on the IFE or EIFE interface, and IFE server cannot be changed.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.