DOCA0162EN-02

Model Implementation Conformance Statement

Introduction

The Model Implementation Conformance Statement (MICS) is defined by IEC 61850-7-3 and IEC 61850-7-4, and provides the following specifications:

  • Logical nodes, used to model substation devices and functions.

  • Common data classes and common data attribute classes used in the logical nodes.

The data requirements are rated as follows:

  • M: Mandatory

  • O: Optional

  • C: Conditional

  • E: Extension

  • X: Supported

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.