DOCA0162EN-02

Reporting Triggers Configuration

The reporting triggers allows the MasterPacT MTZ IED to generate and send reports automatically to clients, when certain conditions are met. They are configured using the CET850 configuration software.

NOTE: It is recommended to set to the default configuration.

The following figure shows the report control block configuration settings:


The list of reporting triggers are:

Reporting triggers

Description

Value/Comments

Supported trigger conditions

Integrity

Supported

Data change

Supported

Data update

Supported (can be set, however there is no process data to report for this condition.)

Quality change

Supported

General interrogation

Supported

Supported optional fields

Sequence Number

Supported

Report time-stamp

Supported

Reason for inclusion

Supported

Dataset name

Supported

Data reference

Supported

Conf-rev

Supported

Segmentation

Not Supported

Sending of segmented reports

Supported

Second change of analogue or digital value during buffer time

Report is sent immediately

Online changeable RCB members

RptID, OptFlds, BufTm, TrgOpts, IntgPd, and RptEna

URCB management

The auto-indexation of the URCB with the use of the RptEnabledmax="n" attribute is supported. Indexed URCBs are visible from all clients

For the complete list of reporting triggers, refer to Abstract Communication Services Interface Conformance Statement.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.