DOCA0162EN-02

IED Identification

@added D2
You must add identification details to the IED before adding it to an IEC 61850 system.

  • ICD/CID file: Select IEC 61850 description of the IED to add by an ICD or a CID.

    NOTE: You can select a device from the library or select any other device with the ICD file.
  • IED name: Assign a name to the IED. The name of the IED is unique in the IEC 61850 system.

    A valid IED name must comply with the below naming convention rules:

    • Can begin with a letter

    • Must contain only alphanumeric and underscore characters.

    • Must not exceed a maximum length of 64 characters.

  • IED description: This is a free ASCII string where you can write comments about the device.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.