DOCA0162EN-02

CID.exi File Transfer to IFE or EIFE Interface with Firmware Version up to V004.005.000 (On-Site Configuration)

The CID.exi file is transferred to IFE or EIFE interface with firmware version ≤ V004.005.000 via the FTP protocol using the CET850 configuration software. The on-site configuration requires Ethernet connection to the IFE or EIFE interface.

NOTE:
  • At a single time, only one CID.exi file can be loaded onto the IEC 61850 folder in IFE or EIFE interface.

  • If the IFE or EIFE interface is reset to the factory setting, the CID.exi file in the IFE or EIFE interface is erased. The IFE or EIFE interface must be retransferred and the CID.exi file has to be retransferred into the IFE or EIFE interface.

The following procedure describes how to transfer IEC 61850 CID.exi file to the IFE or EIFE interface:

Step

Action

1

Run the CET850 configuration software.

2

Enter the IP address of IFE or EIFE interface to get connected to the IFE or EIFE interface through FTP.

NOTE: The previous CID.exi file can be archived as part of historical information of the IED.

3

Enter the login credentials for FTP. On successful credential verification, the CID.exi files will be transferred to IFE or EIFE interface.

NOTE: The transfer of CID.exi files through FTP is password-protected by Role Based Access Control feature in IFE or EIFE interface. Only users with Engineer or Installer roles can transfer the CID.exi files.

4

The IFE or EIFE interface validates the CID.exi file.

NOTE: If the CID.exi file is invalid, the IEC 61850 features of the MasterPacT MTZ IED does not function and the ULP LED will flash for five times to indicate discrepancy in configuration.

5

On successful validation of CID.exi file, it is recommended to disable the FTP settings in the IFE or EIFE webpage.

NOTE: Only users with Administrator role can change the FTP settings.

For more information, refer to the following user guides:

The following figure shows the FTP credentials required for MasterPacT MTZ IED:

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.