DOCA0162EN-02

Add an IED

The CET850 configuration software enables the addition of an IED to an IEC 61850 system using its ICD description file, or the addition of a device already defined by a CID file. A specific dialog interface requests a name for the IED and then its description. The description is provided from an ICD file, a CID file, or an IID file.

The following procedure describes the steps to add an IED to the IEC 61850 system:

Step

Action

1

Create a new SCL file for substation system (for example, My Substation.SCD).

2

From the tree view, select the SCL root element.

3

In the menu bar or in the contextual menu, click Add > IED.

4

Set the IED Identification and Address parameters (optional) according to the descriptions given in the section below.

5

Click OK to validate the operation.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.