DOCA0162EN-02

Overview

CET850 software is a Schneider Electric IEC 61850 configuration software. This software must be used to create, display, modify, or optimize the IEC 61850 configuration of MasterPacT MTZ IEDs.


  1. Create an IEC 61850 configuration using an ICD, IID, or CID file as an input.

  2. Edit an existing CID, SCD, IID, or user-customized ICD file to modify its contents by:

    • Displaying the configuration.

    • Modifying communication parameter values.

    • For MasterPacT MTZ IED, all the report control blocks and datasets are preconfigured.

      NOTE: Modifying these parameter values are not recommended.
  3. Generate a CID file for storing the configuration, which can then be imported to the MasterPacT MTZ IED using CET850 configuration software.

  4. Generate SCD file for storing the configuration which can then be imported to any IEC 61850 configuration tools.

  5. Generate an IID file for storing the specific configuration of an instantiated IED which can then be used by other IEC 61850 system configuration tools.

  6. Load the CID file in the IFE interface, EIFE interface, or IFE server.

    • For IFE or EIFE interface with firmware version ≤ V004.005.000, the CET850 configuration software can be used to transfer the files. Refer to the file transfer procedure.

    • For IFE or EIFE interface with firmware version ≥ V004.006.000, use a FTPS client, such as FileZilla or WinSCP to transfer the files. Refer to the file transfer procedure.

    • For IFE server with firmware version ≥ V005.001.000, use a FTPS client, such as FileZilla or WinSCP to transfer the files. Refer to the file transfer procedure.

For more information, refer to CET850 IEC 61850 Configuration Software - User's Manual.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.