DOCA0162EN-02

Graphical SCL Editor

The CET850 configuration software is a graphical tool that enables to browse an SCL file using a tree view that displays the content of the file in a hierarchical format.

Tree View

The following main sections are displayed in the tree view:

  • Header and History

    This section identifies the SCL configuration file and its version.

  • Communication

    This section contains the definition of all sub-networks defined in the IEC 61850 system, with the list of the connected IEDs. Both client/server and peer-to-peer communication access points are displayed.

  • List of IEDs

    This section contains the definition of all IEDs defined in the IEC 61850 system, such as:

    • Logical Devices (LD)

    • Logical Nodes (LN)

    • Datasets (DS)

    • Report Control Blocks (RCB)

Property View

When an item is selected in the tree view, the property view displays the details of the selected item. You can activate editing operations from the toolbar and contextual menu. There are also specific dialog interfaces to guide you.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.