BQT6904400-03

Installation of the Connecting Busbar for 24 kV

Follow the below steps to install the connecting busbar:

  1. Attach the connecting busbar (1) to the busbar (7), and install the bolt (6) along with washer (5). Refer to Standard Tightening Torques

    .
  2. Install the bolts (3) along with washers (2), and hexagonal nuts (10).

  3. Install the plastic bolt (9) along with plastic washer (8), and plastic hexagonal long nut (4).

  4. Install the box phase barrier (11) on the top of busbar, and install the screws (13) along with washers (12).


Figure 74
Installation of the Connecting Busbar (Sheet 1 of 2)

Figure 74
Installation of the Connecting Busbar (Sheet 2 of 2)

1

Connecting busbar(1)

8

Plastic washer M8

2

Washer M8 x 14

9

Plastic bolt M8

3

Bolt M8 x 14

10

Hexagonal nut M8 x 14

4

Plastic hexagonal long nut M8

11

BOX phase barrier

5

Washer M16

12

Washer M8 x 2

6

Bolt M16

13

Screw M8 x 2

7

Busbar

   
(1) Connecting busbar is not in the scope of Schneider Electric
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?