DOCA0102EN-12

Cybersecurity Recommendations

Overview

The MasterPacT MTZ circuit breaker with its MicroLogic X control unit is a key component of your installation. It offers multiple communication features that bring greater efficiency and flexibility in managing your installation. However the features also make it potentially vulnerable to cyber attacks.

This section lists some of the elementary precautions that you must take to protect the communications paths that give access to information about your installation, and control over it.

The communication paths to protect include:

  • Local access communication paths

    • Wireless Bluetooth Low Energy communication

    • Wireless NFC communication

    • The mini USB port

  • Remote access communication paths

    • The Ethernet network when the IFE or EIFE interface is present

    • The Modbus-SL network when the IFM interface is present

For more detailed information about cybersecurity for MasterPacT MTZ circuit breakers, refer to DOCA0122•• MasterPacT, ComPacT, PowerPacT - Cybersecurity Guide.

General Cybersecurity Recommendations

WARNING
POTENTIAL COMPROMISE OF SYSTEM AVAILABILITY, INTEGRITY, AND CONFIDENTIALITY
  • Change default passwords at first use to help prevent unauthorized access to device settings, controls, and information.
  • Disable unused ports/services and default accounts to help minimize pathways for malicious attackers.
  • Place networked devices behind multiple layers of cyber defenses (such as firewalls, network segmentation, and network intrusion detection and protection).
  • Use cybersecurity best practices (for example, least privilege, separation of duties) to help prevent unauthorized exposure, loss, modification of data and logs, or interruption of services.
Failure to follow these instructions can result in death, serious injury, or equipment damage.

For a general introduction to cybersecurity threats and how to address them, refer to How Can I Reduce Vulnerability to Cyber Attacks?.

Cybersecurity Recommendations for Local Access Communication Paths

To help protect local access communication paths, it is recommended to:

  • Keep locked the enclosure where the MasterPacT MTZ circuit breaker is located so that no unauthorized person can access the MicroLogic X control unit.

Specific Cybersecurity Recommendations for Wireless Bluetooth Low Energy Communication

Data transfers using Bluetooth Low Energy wireless communication are encrypted, therefore the risk of an unauthorized person gaining access to confidential information during transmission is limited.

To protect access to functions accessible through Bluetooth, it is recommended to:

  • Disable Bluetooth communications if you do not want to use Bluetooth.

  • Set the Bluetooth automatic disconnection timer to the minimum time (5 minutes).

  • Make sure that the smartphones running the EcoStruxure Power Device app are password-protected and for professional use only.

  • Do not give away information about the smartphone (telephone number, MAC address) if it is not necessary.

  • Disconnect the smartphone from the Internet during a Bluetooth connection with the MicroLogic X control unit.

  • Do not store confidential or sensitive information on smartphones.

Specific Cybersecurity Recommendations for Wireless NFC Communication

To protect access to data accessible through NFC, it is recommended to make sure that the smartphones running the EcoStruxure Power Device app are password-protected and for professional use only.

Specific Cybersecurity Recommendations for USB Connection

To protect access to functions accessible through a USB connection on the MicroLogic X control unit, it is recommended that:

  • The PCs running the monitoring software are hardened following the guidelines provided in MasterPacT, ComPacT, PowerPacT - Cybersecurity Guide

  • The most up-to-date hardening methods for the operating system are running on your PCs.

Specific Cybersecurity Recommendations for USB OTG Connection

To protect access to functions accessible through a USB OTG connection on the MicroLogic X control unit, it is recommended that:

  • The smartphones running the EcoStruxure Power Device app are hardened following the guidelines provided in MasterPacT, ComPacT, PowerPacT - Cybersecurity Guide

  • The most up-to-date hardening methods for the operating system are running on your smartphones.

Cybersecurity Recommendations for Remote Access Communication Paths Through a Communication Network

When the MasterPacT MTZ circuit breaker is connected to a communication network through the IFE, EIFE or IFM interface, it is recommended to:

  • Follow general security rules to protect your network.

  • Make sure that the PCs running the monitoring software are hardened following the guidelines provided in MasterPacT, ComPacT, PowerPacT - Cybersecurity Guide, and with the most up-to-date hardening methods for the operating system running on your PCs.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.