DOCA0102EN-12

Appendix B: MicroLogic Xi Control Unit Description

Presentation

The MicroLogic Xi control units are MicroLogic X control units without wireless communication capability.

All the information related to the MicroLogic X control unit presented in this guide applies to MicroLogic Xi control units except information about wireless communication.

The differences between the MicroLogic X and MicroLogic Xi control units include:

  • Commercial references

  • MicroLogic Xi front face

  • Communication menu

These differences are described further in this appendix.

Commercial References of MicroLogic Xi Control Unit

Standard

Control units

Commercial reference

IEC

MicroLogic 5.0 Xi

LV857602

MicroLogic 6.0 Xi

LV857603

UL

MicroLogic 3.0 Xi

LV857610

MicroLogic 5.0 Xi

LV857609

MicroLogic 6.0 Xi

LV857608

NOTE: The commercial reference is printed on the front face of the MicroLogic Xi control unit. It also identifies the standard, IEC or UL.

Hardware Versions

The hardware version of the MicroLogic Xi control unit can be determined from its serial number, which is part of the control unit identification number.

MicroLogic Xi control unit exists in the following hardware versions:

MicroLogic Xi control unit serial number Communication

Greater than or equal to ••••••243910001

No wireless communication capability

Less than ••••••243910001

NFC communication capability

MicroLogic Xi Control Unit Description

  1. Ready LED

  2. Service LED

  3. ERMS LED

  4. Graphic display screen

  5. Home button

  6. Three contextual buttons

  7. Escape button ESC

  8. Test button for ground-fault protection (MicroLogic 6.0 Xi)

  9. Test/Reset button for trip cause LEDs and alarms

  10. Mini USB port under rubber cover

  11. Overload and trip cause LEDs

  12. Cover for internal battery

  13. VPS voltage power supply module (optional)

  14. VPS LED to indicate that the VPS module is supplying the control unit

  15. QR code to access product information

  16. Control unit identification number

  17. Control unit type

  18. Sensor plug with the rated current of the circuit breaker

  19. Plastic cover

The MicroLogic Xi control units have no wireless communication capability.

The other features of MicroLogic Xi control units are identical to the features of MicroLogic X control units.

Communication Menu

The Home > Configuration > Communication menu presents the following data:

Level 3

Level 4

Level 5

Parameter name

Communication

Bluetooth

 

Not supported by MicroLogic Xi control unit. Bluetooth is displayed in gray but cannot be selected.

Control mode

Mode

Defines the means to control the opening and closing functions:

  • Manual: (BP command only) pushbutton commands only are accepted

  • Automatic:

    • (Local control)

    • (Remote control) (factory setting)

Display Screen Replacement

The display screen can be replaced. Always replace the display screen with one that corresponds to the control unit type (MicroLogic X with wireless communication or MicroLogic Xi without wireless communication).

For information about replacement of the MicroLogic Xi display screen (commercial reference LV850054WWSP), consult the instruction sheet on the Schneider Electric website: GDE66729.

Replacing the display screen of a MicroLogic X control unit with a MicroLogic Xi display screen (and vice versa) generates the hardware discrepancy event Discrepancy between display and MicroLogic. This discrepancy has no impact on the protections provided by the control unit. The control unit is operational.

Nonetheless, the control unit operation is limited as follows:

The other menus cannot be accessed and control unit firmware update is not possible.

NOTE: Changing or replacing the display screen does not change the communication capability of the control unit:
  • Bluetooth Low Energy communication and NFC communication are not available if a MicroLogic X display screen (commercial reference LV850054SP) is installed on a MicroLogic Xi control unit.

  • A MicroLogic Xi control unit with NFC capability (legacy hardware version) keeps its NFC communication capability in the event that a new display screen is installed.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.