DOCA0102EN-12

Alarms & History Menu

Description

The Alarms & History menu contains the following menus:

Level 1

Level 2

Level 3

Function description

Home

Alarms & History

Alarms n

Displays events of medium and high severity of Entry/Exit type, after the occurrence of the alarm and before the completion. The number n indicates the number of active or held alarms.

Trips are not displayed.

Trips history

Displays the history of trips, with the date and time that the trip occurred.

Alarms history

Displays the history of events of medium and high severity, with the date and time for the following type of events:

  • Pulse-type events with the date and time of occurrence

  • Entry/exit-type events with the date and time of completion

Trips are not displayed in this history.

NOTE: Trip history and alarm history events are listed in chronological order, with the most recent event first.

Alarms Screen

An alarm screen for an active alarm contains the following information:

Screen title: Alarm

Description: up to three lines of text describing the nature of the alarm (medium or high severity event).

Event code

Event status: Occurrence

The date and time that the alarm occurred.

Use the up and down arrows at the bottom of the screen to navigate between active alarm screens.

Trips History Screens

A trips history screen contains the following information:

Screen title: Trips history

Description: up to three lines of text describing the nature of the trip (high severity event).

Event code

Event status: Occurrence

The date and time that the event occurred.

Use the up and down arrows at the bottom of the screen to navigate between trips history screens.

Alarms History Screens

An alarms history screen contains the following information:

Screen title: Alarms history

Description: up to three lines of text describing the nature of the alarm (medium or high severity event).

Event code

Event status:

  • Completed: for Entry/Exit type events.

  • Occurrence: for Pulse type events.

The date and time that the event completed or occurred.

Use the up and down arrows at the bottom of the screen to navigate between alarms history screens.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.