DOCA0102EN-12

Monitoring the Circuit Breaker

Presentation

The monitoring of the circuit breaker consists in monitoring its ability to establish or interrupt a circuit and to provide protection against electrical faults. The MicroLogic X control unit therefore monitors:

When the MicroLogic X control unit detects an incident in one of the monitored functions listed, an event is generated with an orange or red pop-up screen and corresponding event message.

Data Availability

Circuit breaker monitoring state data is available as follows:

  • With EcoStruxure Power Commission software

  • With the EcoStruxure Power Device app through Bluetooth or USB OTG connection

  • On a remote controller using the communication network

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.