DOCA0102EN-12

Monitoring the MicroLogic X Control Unit Service Life

Presentation

The MicroLogic X control unit service life indicator helps anticipate the replacement of the control unit before breakdown. The service life of the control unit is measured from the date of manufacture of the control unit. This date is stored in the memory of the MicroLogic X control unit.

For more information about the service life of the MicroLogic X control unit, refer to DOCA0099•• MasterPacT MTZ - IEC Switch-Disconnectors and Circuit Breakers with MicroLogic X Control Unit - Maintenance Guide.

Operating Principle

The MicroLogic X control unit measures time passed since the date of manufacture of the control unit. When the MicroLogic X control unit service life algorithm calculates a value which is below one of the predefined thresholds (20% and 0%), an event is generated with an orange or red pop-up screen and corresponding event message.

Data Availability

Control unit service life monitoring data is available in the following ways:

  • On the MicroLogic X display screen at Home > Maintenance > Health > MicroLogic

  • With EcoStruxure Power Commission software

  • With the EcoStruxure Power Device app through Bluetooth or USB OTG connection

  • On a remote controller using the communication network

Predefined Events

The MicroLogic X control unit service life monitoring generates the following events:

Code

Event

History

Severity

0x1445 (5189)

Remaining service life of MicroLogic is below alarm threshold

Diagnostic

Medium

0x1446 (5190)

MicroLogic control unit has reached the max service life

Diagnostic

High

Recommended Actions

Code

Event

Recommended actions

0x1445 (5189)

Remaining service life of MicroLogic is below alarm threshold

Plan to replace the MicroLogic X control unit.

To refine this theoretical alarm by taking in account environmental parameters, you may ask for aging diagnostic. If the device is cloud connected, use EcoStruxure Asset Advisor for remote aging diagnostic. Otherwise, contact Schneider Electric services for a local aging diagnostic.

0x1446 (5190)

MicroLogic control unit has reached the max service life

Replace the MicroLogic X control unit.

Contact Schneider Electric Support or your Schneider Electric Services representative for more information about who can carry out the recommended actions.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.