DOCA0102EN-12

Event Display

Introduction

The event status table contains the status of all events at the time of consultation. The status can be inactive, active, or held.

Events which are in the active and held state are displayed on the following interfaces:

  • MicroLogic X display screen.

  • EcoStruxure Power Commission software.

  • EcoStruxure Power Device app.

The status of an event can be checked using the communication network.

Displaying Events on the MicroLogic X Display Screen

Display the active and held events on the MicroLogic X display screen at Home > Alarms & History > Alarms.

High and medium severity active and held events are displayed.

The events are displayed in no specific order, with the description of the event and the time it occurred.

If the event is completed while the screen is open, the message Completed is displayed on the screen.

Displaying Events on EcoStruxure Power Commission Software

High and medium severity, active and held events are displayed.

Events can be sorted by:

  • Date

  • Severity:

    • High severity events

    • Medium severity events

  • History

  • Type

Displaying Events on EcoStruxure Power Device App

By default, events are sorted chronologically. They can be sorted by other parameters such as date, severity, type or history.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.