DOCA0102EN-12

Setting the Directional Overcurrent Protection (ANSI 67)

Setting Guidelines

Directional overcurrent protection is used in conjunction with short-time overcurrent protection. The choice of forward or reverse directional overcurrent protection and time delays (tfw and trv), and the time delay settings of short-time overcurrent protection (tsd) help to protect a power system against short-circuit currents that could circulate in forward and reverse directions.

When directional overcurrent protection is used to trip, instantaneous overcurrent protection (ANSI 50) is usually disabled by setting Ii mode to OFF.

Application on Power System with Multiple Sources in Parallel

Directional overcurrent protection can be applied on a power system with two or more sources running in parallel to increase power availability. The sources can be transformers or generators.

Examples of two power systems are presented, with and without directional overcurrent protection:

  • Two sources running in parallel with no tie circuit breaker.

  • Two sources running in parallel with one tie circuit breaker, with tie circuit breaker normally closed.

Hardware configuration

Protection scheme

Power availability

Example applications

2 sources

No tie

2 circuit breakers without directional overcurrent protection

Commercial and industrial buildings

2 circuit breakers with directional overcurrent protection

**

Commercial and industrial buildings

2 sources

1 tie, normally closed

2 circuit breakers without directional overcurrent protection

1 tie circuit breaker without directional overcurrent protection

*

Oil and gas applications

Marine applications

Data centers

2 circuit breakers with directional overcurrent protection

1 tie circuit breaker without directional overcurrent protection

***

Oil and gas applications

Marine applications

Data centers

Setting Guidelines for Two Sources with No Tie

The following table indicates the settings of the overcurrent protections of the circuit breakers:

Circuit breaker

ANSI 50

ANSI 51

ANSI 67 forward

ANSI 67 reverse

Q1 and Q2 without ANSI 67

OFF

tsd = 0.2 s

N/A

N/A

Q1 and Q2 with ANSI 67

OFF

tsd = 0.2 s

OFF

trv = 0.1 s

Q3

ON

tsd = 0.1 s

N/A

N/A

The following table indicates the behavior of the overcurrent protections depending on the location of the short-circuit current:

Case

Q1 and Q2 without ANSI 67

Q1 and Q2 with ANSI 67

Short-circuit in A1

  • Q1 trips on ANSI 51

  • Q2 trips on ANSI 51

The busbar is OFF.

  • Q1 trips on ANSI 67

    (Irv1<Isd2, trv1<tsd2)

  • Q2 is ON

The busbar is ON.

Short-circuit in B1

  • Q1 trips on ANSI 51

  • Q2 trips on ANSI 51

The busbar is OFF. The addition of a tie circuit breaker can keep half of the busbar ON.

  • Q1 trips on ANSI 51

  • Q2 trips on ANSI 51

The busbar is OFF. The addition of a tie circuit breaker can keep half of the busbar ON.

Setting Guidelines for Two Sources with One Tie

The following table indicates the settings of the overcurrent protections of the circuit breakers:

Circuit breaker

ANSI 50

ANSI 51

ANSI 67 forward

ANSI 67 reverse

Q1 and Q2 without ANSI 67

ON

tsd = 0.3 s

N/A

N/A

Q1 and Q2 with ANSI 67

OFF

tsd = 0.3 s

OFF

trv = 0.1 s

Q12 without ANSI 67

ON

tsd = 0.2 s

N/A

N/A

Q3, Q4

ON

tsd = 0.1 s

N/A

N/A

The following table indicates the behavior of the overcurrent protections depending on the location of the short-circuit current:

Case

Q1, Q2 without ANSI 67

Q1, Q2 with ANSI 67

Short-circuit in A1

  • Q12 trips on ANSI 51

  • Q1 trips on ANSI 51

  • Q2 is ON

Half of the busbar (1) is OFF.

Half of the busbar (2) is ON.

  • Q1 trips on ANSI 67

    (Irv1<Isd2 and Isd12, trv1<tsd2 and tsd12)

  • Q12 is ON

  • Q2 is ON

The busbar is ON.

Short-circuit in B1

  • Q12 trips on ANSI 51

  • Q1 trips on ANSI 51

  • Q2 is ON

Half of the busbar (1) is OFF.

Half of the busbar (2) is ON.

  • Q1 trips on ANSI 51

  • Q2 trips on ANSI 51

Half of the busbar (1) is OFF.

Half of the busbar (2) is ON.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.