DOCA0102EN-12

Instantaneous Overcurrent Protection (I or ANSI 50)

Presentation

Instantaneous protection helps to protect equipment against phase-to-phase, phase-to-neutral and phase-to-ground short circuits. The protection operates with a definite time characteristic. It trips without additional time delay as soon as the setting current is exceeded.

The protection offers two tripping modes, with different breaking times:

  • Standard: breaking time of 50 ms, used for applications requiring selectivity. Full selectivity can be provided with any ComPacT NSX or PowerPacT H-, J-, L-frame circuit breaker installed downstream of a MasterPacT MTZ circuit breaker (Refer to selectivity tables for details for Ue ≤ 440 Vac).

  • Fast: breaking time of 30 ms, typically used for applications where the thermal constraints of the equipment need to be limited and when selectivity is not required. For more information, refer to LVPED318033EN Complementary Technical Information.

NOTE: On MicroLogic 2.0 X, instantaneous protection is based on short-time protection without time setting with standard breaking time of 80 ms.

Availability

Instantaneous overcurrent protection is available on:

  • MicroLogic 2.0 X, 5.0 X, 6.0 X, and 7.0 X control units for IEC standard

  • MicroLogic 3.0 X, 5.0 X, and 6.0 X control units for UL standard

  • 3-pole and 4-pole circuit breakers

It is powered by the current flowing through the internal current transformers of the circuit breaker and it does not require an additional external power supply.

Operating Principle

The instantaneous overcurrent protection threshold sets the level of short-circuit current at which the circuit breaker trips with no intentional time delay.

For MicroLogic 5.0 X, 6.0 X, 7.0 X control units for IEC and UL standards, instantaneous overcurrent protection can be disabled.

For MicroLogic 2.0 X control units for IEC standard and MicroLogic 3.0 X control units for UL standard, instantaneous overcurrent protection cannot be disabled.

Instantaneous overcurrent protection overrides short-time overcurrent protection when the instantaneous overcurrent threshold is adjusted to the same or a lower setting than the short-time overcurrent threshold.

Setting the Protection for MicroLogic 2.0 X

The instantaneous overcurrent protection setting for MicroLogic 2.0 X is:

  • Isd: instantaneous overcurrent protection threshold (corresponds to a short-time overcurrent protection threshold without time setting)

It can be set as follows:

  • On the MicroLogic X display screen, at Home > Protection > I Instantaneous

  • With EcoStruxure Power Commission software (password-protected)

  • With EcoStruxure Power Device app (password-protected)

  • By sending a setting command using the communication network (password-protected).

Instantaneous overcurrent protection can be duplicated when dual settings are activated.

Protection Settings for MicroLogic 2.0 X

Setting

Unit

Range

Step

Factory setting

Isd

A

1.5–10 x Ir

0.5 x Ir(1)

1.5 x Ir

(1) Finer resolution settings are possible with EcoStruxure Power Commission software and EcoStruxure Power Device app.

For more information, refer to the setting guidelines.

Protection Characteristics for MicroLogic 2.0 X

Characteristic

Unit

Value

Breaktime at 2 x Isd threshold

ms

≤ 80

Non-tripping time

ms

> 20

Accuracy on threshold

%

+/- 10

Setting the Protection for MicroLogic 3.0 X

The instantaneous overcurrent protection setting for MicroLogic 3.0 X is:

  • Ii: instantaneous overcurrent protection threshold

It can be set as follows:

  • On the MicroLogic X display screen, at Home > Protection > I Instantaneous

  • With EcoStruxure Power Commission software (password-protected)

  • With EcoStruxure Power Device app (password-protected)

  • By sending a setting command using the communication network (password-protected).

Instantaneous overcurrent protection can be duplicated when dual settings are activated.

Protection Settings for MicroLogic 3.0 X

Setting

Unit

Range

Step

Factory setting

Ii tripping mode

Standard/Fast

Standard

Ii

A

1.5–12 x In

0.5 x In(1)

1.5 x In

(1) Finer resolution settings are possible with EcoStruxure Power Commission software and EcoStruxure Power Device app.

For more information, refer to the setting guidelines.

Protection Characteristics for MicroLogic 3.0 X

Characteristic

Unit

Ii tripping mode is set to Standard

Ii tripping mode is set to Fast

Breaktime at 2 x threshold

ms

≤ 50

≤ 30

Non-tripping time

ms

> 20

0

Accuracy on threshold

%

+/- 10

+/- 10

Setting the Protection for MicroLogic 5.0 X, 6.0 X, 7.0 X

The instantaneous overcurrent protection settings are:

  • Ii mode: enables (ON) or disables (OFF) instantaneous overcurrent protection

  • Ii tripping mode: sets tripping time to standard or fast

  • Ii: instantaneous overcurrent protection threshold

They can be set as follows:

  • On the MicroLogic X display screen, at Home > Protection > I Instantaneous

  • With EcoStruxure Power Commission software (password-protected)

  • With EcoStruxure Power Device app (password-protected)

  • By sending a setting command using the communication network (password-protected).

Instantaneous overcurrent protection can be duplicated when dual settings are activated.

Protection Settings for MicroLogic 5.0 X, 6.0 X, 7.0 X

Setting

Unit

Range

Step

Factory setting

Ii mode

ON/OFF

ON

Ii tripping mode

Standard/Fast

Standard

Ii

A

2.0–15 x In

0.5 x In(1)

2.0 x In

For more information, refer to the setting guidelines.

Protection Characteristics for MicroLogic 5.0 X, 6.0 X, 7.0 X

Characteristic

Unit

Ii tripping mode is set to Standard

Ii tripping mode is set to Fast

Breaktime at 2 x threshold

ms

≤ 50

≤ 30

Non-tripping time

ms

> 20

0

Accuracy on threshold

%

+/- 10

+/- 10

Predefined Events for MicroLogic 2.0 X

The function generates the following predefined events:

Code

Event

History

Severity

0x6401 (25601)

Isd trip

Trip

High

0x6301 (25345)

Isd operate

Protection

Medium

0x6201 (25089)

Isd start

Protection

Low

Predefined events cannot be modified by the user. For general information about events, refer to Event management.

Protection events are generated as follows:

  • The start event is generated when the protection picks up.

  • The operate event is generated when the protection time delay elapses.

  • The trip event is generated when the circuit breaker tripping voltage release (MITOP) activates.

Recommended Actions

Code

Event

Recommended actions

0x6401 (25601)

Isd trip

Reset the device or use the Power restoration assistant within the EcoStruxure Power Device app.

Predefined Events for MicroLogic 3.0 X, 5.0 X, 6.0 X, 7.0 X

The function generates the following predefined events:

Code

Event

History

Severity

0x6402 (25602)

Ii trip

Trip

High

0x6302 (25346)

Ii operate

Protection

Medium

Predefined events cannot be modified by the user. For general information about events, refer to Event management.

Protection events are generated as follows:

  • The operate event is generated when the protection time delay elapses.

  • The trip event is generated when the circuit breaker tripping voltage release (MITOP) activates.

Recommended Actions

Code

Event

Recommended actions

0x6402 (25602)

Ii trip

Reset the device or use the Power restoration assistant within the EcoStruxure Power Device app.

Resetting a Trip Event

For information about resetting the circuit breaker after a trip due to an electrical fault, refer to the relevant document:

  • MasterPacT MTZ1 - Circuit Breakers and Switch-Disconnectors - User Guide

  • MasterPacT MTZ2/MTZ3 - Circuit Breakers and Switch-Disconnectors - User Guide

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.