DOCA0102EN-12

Opening Function

Presentation

MicroLogic X control units receive and process electrical opening orders. An event is generated on opening.

Operating Principle

Opening orders can be sent as follows:

  • Directly through a mechanical opening pushbutton.

  • Locally through an external opening pushbutton.

  • Remotely through a remote order which is managed by the MicroLogic X control unit.

Opening orders have priority over closing orders. No closing orders are taken into account as long as an open order is active.

The open orders on MN or MX voltage releases by external pushbutton can be maintained to force the circuit breaker in open position and reject any close order. The MicroLogic X open orders are not maintained.

Management of Opening Function

DANGER
HAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
  • Do not operate the circuit breaker without confirming that doing so will not create a hazardous situation.
  • Do not allow any person to work on the electrical network without physically validating the successful execution of the local or remote software actions for opening the circuit breaker or switching off the electrical circuit.
Failure to follow these instructions will result in death or serious injury.

The MicroLogic X control unit manages opening orders issued by the following means:

The opening function is monitored by the MicroLogic X control unit.

CB closed

Circuit breaker is closed

Auto: Local

Control mode is Auto Local

EPD open

Open order from EcoStruxure Power Device app with MasterPacT Operation Assistant Digital Module

EPC USB open

Open order from EcoStruxure Power Commission software connected to the mini USB port on control unit

IO local open

Local open order from IO module with the Breaker Operation predefined application (I5)

FDM121 open

Open order from FDM121 display

Auto: Remote

Control mode is Auto Remote

COM open

Open order from a remote controller

Webpage open

Open order from IFE/EIFE webpage

IO remote open

Remote open order from IO module with the Breaker Operation predefined application (I2)

FDM128 open

Open order from FDM128 display

EPC COM open

Open order from EcoStruxure Power Commission software through the communication network

Open

MicroLogic X open order to the MX communicating opening voltage release

Predefined Events

The function generates the following predefined events:

Code

Event

History

Severity

0x1000 (4096)

Circuit breaker opened

Operation

Low

0x0410 (1040)

Opening order sent to MX voltage release

Operation

Low

0x111F (4383)

Allow control by digital input is disabled

Operation

Low

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.