DOCA0102EN-12

MicroLogic X Control Unit: Presentation

MicroLogic X Control Units for IEC and UL Standards - Overview

MasterPacT MTZ circuit breakers with MicroLogic X control units provide functions of protection, metering, diagnostics, communication, and remote operation. The control unit can be customized with optional Digital Modules.

MicroLogic X control units allow operation and monitoring of MasterPacT MTZ circuit breakers locally or remotely.

The MicroLogic X control units for IEC standard are:

  • MicroLogic 2.0 X

  • MicroLogic 5.0 X

  • MicroLogic 6.0 X

  • MicroLogic 7.0 X

The MicroLogic X control units for UL standard are:

  • MicroLogic 3.0 X

  • MicroLogic 5.0 X

  • MicroLogic 6.0 X

Convention

Unless specifically indicated as follows, the information in this guide is valid for both IEC and UL standards:

  • Information indicated for MicroLogic 5.0 X IEC and MicroLogic 6.0 X IEC is valid only for the IEC standard.

  • Information indicated for MicroLogic 5.0 X UL and MicroLogic 6.0 X UL is valid only for the UL standard.

For this guide, electrical phases described as phase 1, phase 2, phase 3 cover both IEC standard and UL standard, with the following equivalence:

IEC standard

UL standard

Phase 1

Phase a

Phase 2

Phase b

Phase 3

Phase c

Range of MicroLogic X Control Units for IEC Standard

The following table indicates the standard functions available on MasterPacT MTZ circuit breakers with MicroLogic X control units for IEC standard:

 

MicroLogic 2.0 X

MicroLogic 5.0 X

MicroLogic 6.0 X

MicroLogic 7.0 X

Commercial reference

LV847600

LV847602

LV847603

LV847604

Long-time overcurrent protection (L)

Short-time overcurrent protection (S)

Instantaneous overcurrent protection (I)

Ground-fault protection (G)

Earth-leakage protection (V)

Neutral protection

Dual settings

Overcurrent and trip cause indicators

Zone selective interlocking

Trip history

Setting change traceability

Embedded power meter class 1

Embedded diagnostics

NOTE: The commercial reference is printed on the front face of the MicroLogic X control unit and also identifies the standard, IEC or UL.

Range of MicroLogic X Control Units for UL Standard

The following table indicates the standard functions available on MasterPacT MTZ circuit breakers with MicroLogic X control units for UL standard:

 

MicroLogic 3.0 X

MicroLogic 5.0 X

MicroLogic 6.0 X

Commercial reference

LV848815

LV847609

LV847608

Long-time overcurrent protection (L)

Short-time overcurrent protection (S)

Instantaneous overcurrent protection (I)

Ground-fault protection (G)

Earth-leakage protection (V)

Neutral protection

Dual settings

Overcurrent and trip cause indicators

Zone selective interlocking

Trip history

Setting change traceability

Embedded power meter class 1

Embedded diagnostics

NOTE: The commercial reference is printed on the front face of the MicroLogic X control unit and also identifies the standard, IEC or UL.

Communication

MicroLogic X control units support wireless and wired communication and enable local and network communication.

Local communication includes:

  • Wireless connection to a smartphone running the EcoStruxure Power Device app through:

    • Bluetooth® Low Energy

    • NFC

  • Wired connection via the mini USB port to:

Network communication includes:

  • Wired connection via the ULP port module (optional) to

    • Ethernet communication network with Modbus TCP/IP and/or IEC 61850 protocols

    • Serial Line communication network with Modbus-SL protocol

MicroLogic X Control Units in Smart Panels

MasterPacT circuit breakers with MicroLogic X control units, in conjunction with Enerlin’X, provide simple and reliable access to data from a smartphone or PC.

MicroLogic X control units communicate using:

  • Modbus TCP/IP protocol on Ethernet through an IFE server, or an IFE or EIFE interface

  • Modbus TCP/IP and IEC 61850 protocols on Ethernet through an IFE or EIFE interface

  • Modbus-SL protocol through an IFM interface with reference LV434000 (IFM interface with reference TRV00210 is not compatible with MasterPacT MTZ circuit breakers).

  • Bluetooth Low Energy or NFC for a wireless connection to the EcoStruxure Power Device app

  • The mini USB port to connect to:

    • A PC running EcoStruxure Power Commission software

    • A smartphone running the EcoStruxure Power Device app (USB OTG connection)

  • A Panel Server and Ethernet to connect to the Internet

The following diagram shows how MicroLogic X control units communicate within a digital system:

Ethernet

USB

USB OTG connection

A FDM121 front display module for one circuit breaker

B FDM128 Ethernet display for eight devices

C IFE/EIFE webpages

D Panel Server

E EIFE interface

F EcoStruxure Power Device app through Bluetooth Low Energy or NFC wireless communication

G EcoStruxure Power Device app through USB OTG connection

H EcoStruxure Power Commission software

I Go2SE landing page

J ULP port module for MasterPacT MTZ circuit breakers

NOTE: The FDM121 display with firmware version greater than or equal to 004.000.009 is compatible with MicroLogic X control units. Earlier firmware versions need to be updated.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.