DOCA0102EN-12

Configuration Menu

Description

The Configuration menu contains the following submenus:

Level 1

Level 2

Level 3

Function description

Home

Configuration

General

Settings of the HMI display and control of access to protection settings.

Network

Settings of nominal voltage and frequency, power sign, and VT ratio.

Measures

Settings of measurement calculation.

Communication

Settings enabling wireless access and the control mode.

General

The General menu presents the following data:

Level 3

Level 4

Level 5

Parameter name

General

Language Display Screen Language

List of display screen languages.

Date & time MicroLogic X Control Unit: Date and Time

dd/mm/yyyy

Set the date.

hh:mm:ss

Set the time.

Quick view Configuring Quick View Mode

Scrolling

Enable/disable Quick View scrolling.

Auto start (min)

The time delay before Quick View scrolling resumes after an interruption if no button is pressed.

NOTE: Only available when Quick View scrolling is enabled.

Pageflow (s)

The length of time (in seconds) for which each Quick View screen is displayed.

NOTE: Only available when Quick View scrolling is enabled.

Time out (min)

The time delay before the Quick View Current screen is displayed if no button is pressed.

NOTE: Only available when Quick View scrolling is not enabled.

Lock protection Enabling and Disabling Access to Protection Settings

Keypad

Enable locking of local access to the Protection menu through the MicroLogic X keypad. This helps to prevent unauthorized users from editing protection settings.

  • Protection change > Allowed means that the Protection menu can be accessed from the MicroLogic X keypad.

  • Protection change > Not allowed means that the Protection menu cannot be accessed from the MicroLogic X keypad.

External access

Enable locking of external access to the Protection menu. This helps to prevent unauthorized users from editing protection settings.

  • Protection change > Allowed means that the Protection menu can be externally accessed.

  • Protection change > Not allowed means that the Protection menu cannot be externally accessed.

Pop-up messages Auto-acknowledgement of Pop-up Messages Auto Acknowledge

Auto-acknowledgment mode for predefined medium severity events displayed in an orange pop-up screen:

  • ON

  • OFF (factory setting)

Pop-up delay (s)

Time delay before pop-up is acknowledged automatically when auto-acknowledgment mode is ON.

  • Setting range: 1–250 s

  • Factory setting = 15 s

Network

The Network menu presents the following data:

Level 3

Level 4

Level 5

Parameter name

Network

Nominal voltage

Vn (V)

Rated voltage.

Setting values include: 208 / 220 / 230 / 240 / 380 / 400 / 415 / 440 / 480 / 500 / 525 / 550 / 575 / 600 / 660 / 690 / 1000 V.

Factory setting = 400.

Nominal frequency

Hz

Rated frequency

  • 50 Hz (factory setting)

  • 60 Hz

Power sign Power Sign Convention

Power flow sign setting:

  • P+ = the active power flows from upstream (top) to downstream (bottom) (factory setting).

  • P– = the active power flows from downstream (bottom) to upstream (top).

VT ratio

VT in

VT primary voltage.

Values from 100 to 1,250, in increments of 1.

VT out

VT secondary voltage.

Values from 100 to 690, in increments of 1.

Measures

The Measures menu presents the following data:

Level 3

Level 4

Level 5

Parameter name

Measures

PF/Var Selecting the Sign Convention for the cos φ and Power Factor PF

Sign convention for cos φ, PF power factor, and reactive power:

  • IEC

  • IEEE (factory setting)

System type System Type Setting

Nb poles

3P or 4P, for display only.

ENVT

External neutral voltage tap. Setting values include:

  • If 4P: NO (for display only)

  • If 3P: NO or YES (factory setting)

ENCT

External neutral current transformer. Setting values include:

  • If 4P: NO (for display only)

  • If 3P: NO (factory setting) or YES

Tot. P calcul Total Power Calculation Method

Total power calculation method:

  • Vector

  • Arithmetic (factory setting)

E calcul Selecting Energy Calculation

Energy Accumulation mode. Energy values to be used in energy calculations:

  • Absolute (factory setting)

  • Signed

Communication

The Communication menu presents the following data:

Level 3

Level 4

Level 5

Parameter name

Communication

Bluetooth(1)

ON

Enables Bluetooth control

OFF (factory setting)

Disables Bluetooth control

Timer (min)

Time delay before Bluetooth is automatically deactivated:

  • If no connection is established

  • If no activity is detected

From 5 to 60 minutes.

Factory setting = 15 minutes

Control mode

Mode

Defines the means to control the opening and closing functions:

  • Manual: (BP command only) pushbutton commands only are accepted

  • Automatic:

    • (Local control)

    • (Remote control) (factory setting)

(1) The Bluetooth menu cannot be selected on MicroLogic Xi control units.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.