DOCA0102EN-12

Monitoring the Load Profile

Presentation

Four load profile counters report the number of hours during which the MicroLogic X control unit has measured current flowing through the circuit breaker, in the following In ratio ranges:

  • Number of hours with current measured between 0 and 49% of the rated current In

  • Number of hours with current measured between 50 and 79% of the rated current In

  • Number of hours with current measured between 80 and 89% of the rated current In

  • Number of hours with current measured at 90% of the rated current In or above

Data Availability

Load profile monitoring data is available as follows:

  • With EcoStruxure Power Commission software

  • With the EcoStruxure Power Device app through Bluetooth or USB OTG connection

  • On the FDM128 display

  • On the FDM121 display

  • On a remote controller using the communication network.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.