DOCA0102EN-12

Measures Menu

Presentation

In this guide, electrical phases are described as phase 1, phase 2, phase 3 and cover both IEC standard and UL standard. The MicroLogic X control unit displays the phases as follows:

MicroLogic X control unit for IEC standard

MicroLogic X control unit for UL standard

Phase 1

Phase a

Phase 2

Phase b

Phase 3

Phase c

Description

The Measures menu contains the following submenus:

Level 1

Level 2

Level 3

Function description

Home

Measures

Current

Current real-time measurements

Voltage

Voltage real-time measurements

Power

Power real-time measurements

Energy

Energy real-time measurements

Frequency

Frequency real-time measurements

I harmonics

Current harmonics real-time measurements

V harmonics

Voltage harmonics real-time measurements

Power factor

Power factor real-time measurements

Measures Screens with Quality Gauge

A quality gauge is displayed on the following screens to give a graphical representation of the measurement compared to the expected range:

  • Real-time maximum of 3 phase current unbalances, Iunb

  • Average of 3 RMS phase-to-phase voltages Vavg VLL(V)

  • Real-time maximum of 3 phase-to-phase voltage unbalances Vunb VLL(%)

  • Frequency F(Hz)

For example, for the frequency screen, the following icons indicate the measurement compared to the expected range:

Measurement OK: the difference between the measured and expected frequencies is less than 1%

Measurement out of range: the difference between the measured and expected frequencies is +1–4% or -1– -6%

Measurement significantly out of range: the difference between the measured and expected frequencies is greater than +4% or less than -6%

Current

The Current menu presents the following measurements:

Level 3

Level 4

Level 5

Parameter name

Current

I

I1 (A)

RMS current on phase 1

I2 (A)

RMS current on phase 2

I3 (A)

RMS current on phase 3

IN (A)(1)

RMS current on neutral

Ig (A)(2)

RMS current on ground

IΔn (A)(3)

RMS current on earth leakage

I MAX

I1 (A)

Maximum RMS current on phase 1

I2 (A)

Maximum RMS current on phase 2

I3 (A)

Maximum RMS current on phase 3

IN (A)(1)

Maximum RMS current on neutral

Ig (A)(2)

Maximum of RMS current on ground

IΔn (A)(3)

Maximum of RMS current on earth leakage

I avg

I (1,2,3) (A)

Average of 3 phase RMS currents

I unb

I (1,2,3) (%)

Real-time maximum of 3 phase current unbalances, with quality gauge

I unb MAX

I (1,2,3) (%)

Maximum of maximum of 3 phase current unbalances

Reset MAX

Reset of maximum RMS current, with date and time of last reset

(1) Applies to 4-pole circuit breakers or 3-pole circuit breakers with ENCT wired and configured

(2) Applies to MicroLogic 2.0 X, 3.0 X, 5.0 X, 6.0 X

(3) Applies to MicroLogic 7.0 X

Voltage

The Voltage menu presents the following measurements:

Level 3

Level 4

Level 5

Parameter name

Voltage

V

V12 (V)

RMS phase-to-phase voltage 1-2

V23 (V)

RMS phase-to-phase voltage 2-3

V31 (V)

RMS phase-to-phase voltage 3-1

V1N (V)(1)

RMS phase-to-neutral voltage 1-N

V2N (V)(1)

RMS phase-to-neutral voltage 2-N

V3N (V)(1)

RMS phase-to-neutral voltage 3-N

V MAX

V12 (V)

Maximum RMS phase-to-phase voltage 1-2

V23 (V)

Maximum RMS phase-to-phase voltage 2-3

V31 (V)

Maximum RMS phase-to-phase voltage 3-1

V1N (V)(1)

Maximum RMS phase-to-neutral voltage 1-N

V2N (V)(1)

Maximum RMS phase-to-neutral voltage 2-N

V3N (V)(1)

Maximum RMS phase-to-neutral voltage 3-N

V MIN

V12 (V)

Minimum RMS phase-to-phase voltage 1-2

V23 (V)

Minimum RMS phase-to-phase voltage 2-3

V31 (V)

Minimum RMS phase-to-phase voltage 3-1

V1N (V)(1)

Minimum RMS phase-to-neutral voltage 1-N

V2N (V)(1)

Minimum RMS phase-to-neutral voltage 2-N

V3N (V)(1)

Minimum RMS phase-to-neutral voltage 3-N

V avg

VLL (V)

Average of 3 RMS phase-to-phase voltages (V12+V23+V31)/3, with quality gauge

VLN (V)(1)

Average of 3 RMS phase-to-neutral voltages (V1N+V2N+V3N)/3

V unb

VLL (%)

Real-time maximum of 3 phase-to-phase voltage unbalances, with quality gauge

VLN (%)(1)

Real-time maximum of 3 phase-to-neutral voltage unbalances

V unb MAX

VLL (%)

Maximum of maximum of 3 phase-to-phase voltage unbalances

VLN (%)(1)

Maximum of maximum of 3 phase-to-neutral voltage unbalances

Reset MIN/MAX

Reset of minimum and maximum RMS voltage, with date and time of last reset

(1) Applies to 4-pole circuit breakers or 3-pole circuit breakers with ENVT wired and configured.

Power

The Power menu presents the following measurements:

Level 3

Level 4

Level 5

Parameter name

Power

P

P1 (kW)

Active power on phase 1

P2 (kW)

Active power on phase 2

P3 (kW)

Active power on phase 3

Ptot (kW)

Total active power

P MAX

Ptot (kW)

Maximum total active power

Q

Q1 (kVAR)(1)

Reactive power on phase 1

Q2 (kVAR)(1)

Reactive power on phase 2

Q3 (kVAR)(1)

Reactive power on phase 3

Qtot (kVAR)

Total reactive power

Q MAX

Qtot (kVAR)

Maximum total reactive power

S

S1 (kVA)(1)

Apparent power on phase 1

S2 (kVA)(1)

Apparent power on phase 2

S3 (kVA)(1)

Apparent power on phase 3

Stot (kVA)

Total apparent power

S MAX

Stot (kVA)

Maximum total apparent power

Reset MAX

Reset of maximum power, with date and time of last reset

(1) Applies to 4-pole circuit breakers or 3-pole circuit breakers with ENVT wired and configured.

Energy

The Energy menu presents the following measurements:

Level 3

Level 4

Level 5

Parameter name

Energy

E total

Ep (kWh)

Total active energy

Eq (kVArh)

Total reactive energy

Es (kVAh)

Total apparent energy

E delivered

Ep (kWh)

Total active energy delivered into the load (counted positively)

Eq (kVArh)

Total reactive energy delivered into the load (counted positively)

E received

Ep (kWh)

Total active energy received out of the load (counted negatively)

Eq (kVArh)

Total reactive energy received out of the load (counted negatively)

Reset counters

Reset of accumulated energy, with date and time of last reset

Frequency

The Frequency menu presents the following measurements:

Level 3

Level 4

Level 5

Parameter name

Frequency

F

F (Hz)

Frequency with quality gauge

F MAX

F (Hz)

Maximum frequency

F MIN

F (Hz)

Minimum frequency

Reset MIN/MAX

Reset of minimum and maximum frequency, with date and time of last reset

I Harmonics

The I harmonics menu presents the following measurements:

Level 3

Level 4

Level 5

Parameter name

I harmonics

I THD

I1 (%)

Total Harmonic Distortion (THD) of current on phase 1 compared to the fundamental

I2 (%)

Total Harmonic Distortion (THD) of current on phase 2 compared to the fundamental

I3 (%)

Total Harmonic Distortion (THD) of current on phase 3 compared to the fundamental

IN (%)(1)

Total Harmonic Distortion (THD) of current on neutral compared to the fundamental

I THD IN MAX(1)

IN (%)

Maximum of Total Harmonic Distortion (THD) of current on neutral compared to the fundamental

I THD avg

I (1, 2, 3) (%)

Average of 3 phase current Total Harmonic Distortions (THD) compared to the fundamental

I THD avg MAX

I (1, 2, 3) (%)

Maximum average of 3 phase current Total Harmonic Distortions (THD) compared to the fundamental, with date and time of occurrence

Reset MAX

Reset of minimum and maximum THD, with date and time of last reset

(1) Applies to 4-pole circuit breakers or 3-pole circuit breakers with ENVT wired and configured.

V Harmonics

The V harmonics menu presents the following measurements:

Level 3

Level 4

Level 5

Parameter name

Voltage

V THD

V12 (%)

Total harmonic distortion (THD) of phase-to-phase voltage 1-2 compared to the fundamental

V23 (%)

Total harmonic distortion (THD) of phase-to-phase voltage 2-3 compared to the fundamental

V31 (%)

Total harmonic distortion (THD) of phase-to-phase voltage 3-1 compared to the fundamental

V1N (%)(1)

Total harmonic distortion (THD) phase-to-neutral voltage 1-N compared to the fundamental

V2N (%)(1)

Total harmonic distortion (THD) phase-to-neutral voltage 2-N compared to the fundamental

V3N (%)(1)

Total harmonic distortion (THD) phase-to-neutral voltage 3-N compared to the fundamental

V THD avg

VLL (%)

Average of 3 phase-to-phase voltage Total Harmonic Distortions (THD) compared to the fundamental

VLN (%)(1)

Average of 3 phase-to-neutral voltage Total Harmonic Distortions (THD) compared to the fundamental

V THD avg MAX

VLL (%)

Maximum value since last reset of average of 3 phase-to-phase voltage Total Harmonic Distortions (THD) compared to the fundamental

VLN (%)(1)

Maximum value since last reset of average of 3 phase-to-neutral voltage Total Harmonic Distortions (THD) compared to the fundamental

Reset MAX

Reset all maximum and minimum voltages

(1) Applies to 4-pole circuit breakers or 3-pole circuit breakers with ENVT wired and configured.

Power Factor Menu

The Power factor menu presents the following data:

Level 3

Level 4

Parameter name

Power Factor

PF

Total power factor

Cos φ

Total fundamental power factor

Network

The parameters displayed depend on the sign convention for power factor and cos phi selected.

  • If IEEE is selected (factory setting), the displayed parameter is:

    • Leading in the case of lead

    • Lagging in the case of lag

  • If IEC is selected, the displayed parameter is:

    • Capacitive in the case of lead

    • Inductive in the case of lag

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.