DOCA0102EN-12

Measurement Accuracy in Accordance with IEC 61557-12

Measurements and Electrical Parameters Available on the MicroLogic X Control Unit

Based on the measurement of line currents, neutral current, phase-to-phase voltages, and phase-to-neutral voltages, the MicroLogic X control unit displays the following parameters:

  • RMS values of currents and voltages

  • Active, reactive, and apparent powers

  • Active, reactive, and apparent energies

  • Power factor

  • Frequency

  • Unbalance, THD, and THD-R of voltages and currents

Average values are calculated for the main basic electrical parameters.

The maximum and minimum values are time stamped and logged in the MicroLogic X non-volatile memory. They can be reset as follows:

  • On the MicroLogic X display screen

  • With EcoStruxure Power Commission software

  • On the FDM128 display

  • On the FDM121 display

  • By a remote controller using the communication network

  • On the IFE/EIFE webpages

Electrical parameters are refreshed once a second. They can be displayed as follows:

  • On the MicroLogic X display screen, at Home > Measures Measures Menu

  • With the EcoStruxure Power Device app

  • With EcoStruxure Power Commission software

  • On the FDM128 display

  • By a remote controller using the communication network

  • On the IFE/EIFE webpages

The availability of parameters depends on the type of interface used to display data. All parameters are not displayed on all interfaces.

An optional external 24 Vdc supply or VPS module is mandatory to measure and display parameters, including energy counters, for currents below 20% of the rated current In.

The start-up time is the time between when the control unit is energized and the availability of the first measurement. The start-up time is less than or equal to 45 seconds.

Measurement Accuracy

Power and energy metering accuracy in MasterPacT MTZ circuit breakers with MicroLogic X control unit is classified as Class 1, according to IEC 61557-12. This standard specifies performance requirements of measuring and monitoring devices that measure and monitor the electrical parameters within electrical distribution systems. It covers both performance measuring devices with external sensors (PMD-S), such as current and/or voltage transformers, for example, stand-alone power meters, and performance measuring devices with embedded sensors (PMD-D), for example, circuit breakers.

A MasterPacT MTZ circuit breaker, with MicroLogic X control unit and embedded sensors, is a PMD-DD device with Class 1 accuracy, according to IEC 61557-12 for power and energy metering. It complies with the requirements of K70 temperature class and ‘Standard’ humidity and altitude operating conditions, according to table 6 and 7 of IEC 61557-12.

The IEC 61557-12 standard defines the following three levels of uncertainty that need to be checked to establish accuracy class:

A PMD-DD device avoids overall system uncertainty and variation, thanks to its embedded sensors and wiring.

Measured Electrical Parameter Uncertainty

Uncertainty is the estimated percentage by which a measured electrical parameter may differ from the true electrical parameter. In the context of this standard, the total uncertainty of a measured electrical parameter depends on the instrument, the environment, and other elements to be considered.

The following graphic shows the total uncertainty of a measured electrical parameter made by:

  • A PMD-D device, with embedded sensors

  • A PMD-S device, with external sensors

PMD-D device, with embedded sensors

PMD-S device, with external sensors

A Uncertainty under reference conditions: Intrinsic uncertainty according to IEC 61557-12

B Variations due to influence quantity: Operating Uncertainty according to IEC 61557-1; Measurement uncertainty according to IEC 61000-4-30

C Overall system uncertainty according to IEC 61557-12

Intrinsic Uncertainty: IEC 61557-12 Definition

Intrinsic uncertainty is the uncertainty of a measuring instrument when used under reference conditions. In the context of this standard, it is a percentage of the measured electrical parameter defined within the rated range of the measuring instrument.

For MasterPacT MTZ circuit breakers with a MicroLogic X control unit, the main values are current and power factor.

The following table indicates, for different MasterPacT MTZ circuit breakers, the current values for an intrinsic uncertainty less than or equal to 1%:

Current values for active power with 1% uncertainty (in A)

MasterPacT

Description of current value

Current value

MTZ1

MTZ2

MTZ3

Lowest value of the current at which the circuit breaker starts and continues to register

Ist = 0.04% Ib

1.6 A

1.6 A

3.2 A

Lowest value of the current for accuracy less than or equal to 1.5% for active power and energy

5% Ib

20 A

20 A

40 A

Lowest value of the current for accuracy less than or equal to 1% for active power and energy with PF = 1

10% Ib

40 A

40 A

80 A

Lowest value of the current for accuracy less than or equal to 1% for active power and energy with PF = 0.5 Inductive to 0.8 Capacitive

20% Ib

80 A

80 A

160 A

Value of current in accordance with which the relevant performance of a direct connected PMD (PMD Dx) is fixed

Ib

400 A

400 A

800 A

Highest value of current at which the MasterPacT MTZ circuit breaker meets the uncertainty requirements of this standard

Imax

1,600 A x 1.2

4,000 A x 1.2

6,300 A x 1.2

The following graph gives an example of the intrinsic uncertainty for active power and energy versus current for the MasterPacT MTZ2 circuit breaker. It shows that the performance of the MasterPacT MTZ2 circuit breaker is equal to or better than the IEC 61557-12 standard.

MasterPacT MTZ2 circuit breaker

IEC 61557-12 standard

Out of IEC 61557-12 standard

Operating Uncertainty

IEC 61557-12 defines operating uncertainty as uncertainty under the rated operating conditions.

IEC 61557-12 specifies tests and maximum variation of uncertainty according to the following influence quantities:

  • Ambient temperature (T°)

  • Frequency, unbalance, harmonics, EMC

For MasterPacT MTZ circuit breakers with MicroLogic X control unit, the main influence quantity is temperature. MasterPacT MTZ circuit breakers are designed to carry high currents, which induce self-heating. The measurement has been designed to offer high stability in a wide range of temperatures.

Effect of Temperature on MasterPacT MTZ Measurement System

The temperature variation around the internal current transformer and the MicroLogic X control unit, between minimum current and nominal current load can be up to 90 K. The effect of temperature on measurement accuracy has been carefully managed over an operating ambient temperature range of -25 °C (-13 °F) to 70 °C (158 °F).

Uncertainty min/max PF 1

Uncertainty min/max PF 0.5

MasterPacT MTZ circuit breaker

IEC 61557-12 standard

Out of IEC 61557-12 standard

Effect of Electromagnetic Compatibility (EMC) and Other Influence Quantities on MasterPacT MTZ Measurement Performance

MasterPacT MTZ circuit breakers with MicroLogic X control unit offer a high immunity to influence quantities, with a low operating uncertainty for active power, as specified by Class 1, for a wide range of operating conditions.

The following table summarizes standard requirements and MasterPacT MTZ performance regarding influence quantities for active power:

Influence quantity

Table 9 IEC 61557-12 PMD DD Cl 1 additional uncertainty variation tolerance

MasterPacT MTZ additional uncertainty

Ambient temperature

PF 1

0.05% / K

< 0.01% / K

PF 0.5 Ind

0.07% / K

< 0.01% / K

Auxiliary power supply

24 Vdc ±15%

0.1%

0%

Voltage

PF 1: 80%/120% Vn

0.7%

0%

PF 0.5 Ind: 80%/120% Vn

1%

0%

Frequency

PF 1: 49–51 Hz/59–61 Hz

0.5%

0%

PF 0.5: 49–51 Hz/59–61 Hz

0.7%

0%

Reversed phase sequence

1.5%

0%

Voltage unbalance

0 to 10%

2%

0%

Phase missing

1 or 2 phase missing

2%

0%

Harmonics in current and voltage

10% Vn 5th

0.8%

< 0.1%

20% Imax 5th

Odd harmonic in current

3%

< 0.1%

Sub harmonic in current

3%

< 0.1%

Common mode voltage rejection

0–690 Vac/ground

0.5%

0%

Permanent ac magnetic induction

IEC 61326

2%

0%

Electromagnetic RF fields

IEC 61326

2%

< 1%

Conducted disturbances induced by RF fields

IEC 61326

2%

< 1%

Overall System Uncertainty

IEC 61557-12 defines overall system uncertainty as uncertainty including the instrumental uncertainty of several separated instruments (for example, sensors, wires, measuring instruments) under the rated operating conditions.

For MasterPacT MTZ circuit breakers, the sensors are embedded in the device for applications up to 690 Vac phase-to-phase and the overall uncertainty is equal to the operating uncertainty.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.