DOCA0102EN-12

Monitoring the Operating Time

Presentation

Two operating times are measured by the MicroLogic X control unit:

  • Operating time with load: total time since energization of the control unit with current flowing through the circuit breaker.

  • Operating time: total time when control unit is powered on by:

    • Current flowing through the circuit breaker

    • External 24 Vdc power supply

    • External power source connected through mini USB port on the front face of the MicroLogic X control unit

Data Availability

Data is available on a remote controller using the communication network.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.