DOCA0102EN-12

Monitoring the Communicating Voltage Releases

Presentation

The voltage releases undergo wear due to the number of opening or closing operations. It is recommended to check them at periodic intervals to decide whether they must be changed or not. To avoid regular inspection of the communicating voltage releases, events are generated when the communicating voltage releases reach 80% or 100% of the recommended maximum number of operations.

The following communicating voltage releases are monitored by MicroLogic X control unit:

  • The diagnostic MN undervoltage release (MN diag).

  • The diagnostic and communicating MX1 opening voltage release (MX1 diag&com).

  • The diagnostic and communicating MX2 opening voltage release (MX2 diag&com).

  • The diagnostic and communicating XF closing voltage release (XF diag&com).

NOTE: Standard voltage releases are not monitored by the MicroLogic X control unit.

Operating Principle

The MicroLogic X control unit:

  • Checks the presence of voltage releases

  • Counts the number of operations performed by the voltage release

  • Calculates the percentage of wear of each voltage release

  • Generates an event when:

    • The voltage release reaches 80% of recommended maximum number of operations

    • The voltage release reaches 100% of recommended maximum number of operations

  • Monitors the state of the internal circuit of the voltage release

For more information about the recommended number of operations, refer to DOCA0099•• MasterPacT MTZ - IEC Switch-Disconnectors and Circuit Breakers with MicroLogic X Control Unit - Maintenance Guide.

Resetting the Counters

NOTICE
invalid monitoring
After replacement of a communicating voltage release, reset the corresponding operation counter to zero.
Failure to follow these instructions will result in incorrect operation count.

The communicating voltage release counters can be reset or set to zero with EcoStruxure Power Commission software (password-protected).

The following voltage release counters can be reset.

  • MN diag undervoltage release operation counter

  • MX1 diag&com opening voltage release operation counter

  • MX2 diag&com opening voltage release operation counter

  • XF diag&com closing voltage release operation counter

Data Availability

The communicating voltage release data is available as follows:

  • On the MicroLogic X display screen, at: Home > Maintenance > Health > Actuator wear

  • With EcoStruxure Power Commission software

  • With the EcoStruxure Power Device app through Bluetooth or USB OTG connection

  • On a remote controller using the communication network

Monitoring data MicroLogic X HMI EPC software EPD app Communication

Percentage wear

Yes

No

Yes

No

Operation counters

No

Yes

No

No

Predefined Events

The monitoring of the communication voltage releases generates the following events:

Code

Event

History

Severity

0x1460 (5216)

Invalid self test - MX1 voltage release

Diagnostic

Medium

0x1461 (5217)

MX1 voltage release not detected

Diagnostic

Medium

0x1452 (5202)

MX1 voltage release operation counter is above alarm threshold

Diagnostic

Medium

0x1453 (5203)

MX1 voltage release has reached the max number of operations

Diagnostic

High

0x1468 (5224)

Invalid self test - MX2 voltage release

Diagnostic

Medium

0x1469 (5225)

MX2 voltage release not detected

Diagnostic

Medium

0x1458 (5208)

MX2 voltage release operation counter is above alarm threshold

Diagnostic

Medium

0x1459 (5209)

MX2 voltage release has reached the max number of operations

Diagnostic

High

0x1464 (5220)

Invalid self test - MN undervoltage release

Diagnostic

Medium

0x1465 (5221)

MN undervoltage release not detected

Diagnostic

Medium

0x1456 (5206)

MN undervoltage release operation counter is above alarm threshold

Diagnostic

Medium

0x1457 (5207)

MN undervoltage release has reached the max number of operations

Diagnostic

High

0x1466 (5222)

Voltage loss on MN undervoltage release

Diagnostic

Medium

0x1467 (5223)

Communication loss on MN undervoltage release

Diagnostic

Medium

0x1462 (5218)

Invalid self test - XF voltage release

Diagnostic

Medium

0x1463 (5219)

XF voltage release not detected

Diagnostic

Medium

0x1454 (5203)

XF voltage release operation counter is above alarm threshold

Diagnostic

Medium

0x1455 (5205)

XF voltage release has reached the max number of operations

Diagnostic

High

Recommended Actions

Code

Event

Recommended actions

0x1460 (5216)

Invalid self test - MX1 voltage release

Plan to replace the MX1 voltage release.

0x1461 (5217)

MX1 voltage release not detected

Check the connection of the MX1 voltage release.

0x1452 (5202)

MX1 voltage release operation counter is above alarm threshold

Plan to replace the MX1 voltage release.

0x1453 (5203)

MX1 voltage release has reached the max number of operations

Replace the MX1 voltage release.

0x1468 (5224)

Invalid self test - MX2 voltage release

Replace the MX2 voltage release.

0x1469 (5225)

MX2 voltage release not detected

Check the connection of the MX2 voltage release.

0x1458 (5208)

MX2 voltage release operation counter is above alarm threshold

Plan to replace the MX2 voltage release.

0x1459 (5209)

MX2 voltage release has reached the max number of operations

Replace the MX2 voltage release.

0x1464 (5220)

Invalid self test - MN undervoltage release

Plan to replace the MN undervoltage release.

0x1465 (5221)

MN undervoltage release not detected

Check the connection of the MN undervoltage release.

0x1456 (5206)

MN undervoltage release operation counter is above alarm threshold

Plan to replace the MN undervoltage release.

0x1457 (5207)

MN undervoltage release has reached the max number of operations

Replace the MN undervoltage release.

0x1466 (5222)

Voltage loss on MN undervoltage release

Check the control voltage.

0x1467 (5223)

Communication loss on MN undervoltage release

Check the internal connection of MN undervoltage release.

0x1462 (5218)

Invalid self test - XF voltage release

Plan to replace the XF voltage release.

0x1463 (5219)

XF voltage release not detected

Check the connection of the XF voltage release.

0x1454 (5204)

XF voltage release operation counter is above alarm threshold

Plan to replace the XF voltage release.

0x1455 (5205)

XF voltage release has reached the max number of operations

Replace the XF voltage release.

Contact Schneider Electric Support or your Schneider Electric Services representative for more information about who can carry out the recommended actions.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.