DOCA0102EN-12

Measurement Availability

Presentation

Measurements can be displayed through the following interfaces:

  • On the MicroLogic X display screen

  • With the EcoStruxure Power Device app (EPD) through Bluetooth or USB OTG connection.

  • With EcoStruxure Power Commission (EPC) software

  • On the FDM128 display

  • On the FDM121 display

  • By a remote controller using the communication network

  • On the IFE/EIFE webpages

The following tables indicate which measurements are displayed on each interface.

Current

The availability of parameters depends on the type of interface used to display data. All parameters are not displayed on all interfaces.

Measurement

MicroLogic X HMI

EPD app

EPC software

FDM128

FDM121

Communication

IFE/EIFE webpages

Real-time phase current values I1, I2, I3

Maximum phase current values I1 MAX, I2 MAX, I3 MAX

Real-time maximum of RMS current of phases I1, I2, I3, IN

Maximum of maximum phase current values

Minimum phase current values I1 MIN, I2 MIN, I3 MIN

Minimum of minimum phase current values

Real-time neutral current value IN(1)

Maximum neutral current value IN MAX(1)

Minimum neutral current value IN MIN(1)

Real-time average current value Iavg

Maximum average current value Iavg MAX

Minimum average current value Iavg MIN

Real-time ground-fault current value

Maximum value of the ground-fault current

Minimum value of the ground-fault current

Real-time earth-leakage current value(2)

Maximum value of the earth-leakage current(2)

(1) Applies to 4-pole circuit breakers or 3-pole circuit breakers with ENCT wired and configured.

(2) Applies to MicroLogic 7.0 X control unit. Values for current related to ground-fault current Ig are not available.

Current Unbalance

Measurement

MicroLogic X HMI

EPD app

EPC software

FDM128

FDM121

Communication

IFE/EIFE webpages

Real-time phase current unbalance values I1 unbal, I2 unbal, I3 unbal

Maximum values of the 3 phase current unbalances l1 unbal MAX, I2 unbal MAX, I3 unbal MAX

Real-time maximum of 3 phase current unbalances

Maximum of maximum of 3 phase current unbalances

Voltage

Measurement

MicroLogic X HMI

EPD app

EPC software

FDM128

FDM121

Communication

IFE/EIFE webpages

Real-time phase-to-phase voltage values V12, V23, V31

Maximum values of phase-to-phase voltages V12 MAX, V23 MAX, V31 MAX

Minimum values of phase-to-phase voltages V12 MIN, V23 MIN, V31 MIN

Real-time phase-to-neutral voltages V1N, V2N, V3N(1)

Maximum values of phase-to-neutral voltages V1N MAX, V2N MAX, V3N MAX(1)

Minimum values of phase-to-neutral voltages V1N MIN, V2N MIN, V3N MIN(1)

Real-time average phase-to-phase voltage Vavg LL

Maximum average phase-to-phase voltage Vavg LL MAX

Minimum average phase-to-phase voltage Vavg LL MIN

Real-time average phase-to-neutral voltage Vavg LN(1)

Maximum average phase-to-neutral voltage Vavg LN MAX(1)

Minimum average phase-to-neutral voltage Vavg LN MIN(1)

(1) Applies to 4-pole circuit breakers or 3-pole circuit breakers with ENVT wired and configured.

Voltage Unbalance

Measurement

MicroLogic X HMI

EPD app

EPC software

FDM128

FDM121

Communication

IFE/EIFE webpages

Real-time phase-to-phase voltage unbalances V12unbal, V23unbal, V31unbal

Maximum values of the 3 phase-to-phase voltage unbalances V12unbal MAX, V23unbal MAX, V31unbal MAX

Real-time maximum of 3 phase-to-phase voltage unbalances

Maximum of maximum of 3 phase-to-phase voltage unbalances

Real-time phase-to-neutral voltage unbalances V1Nunbal, V2Nunbal, V3Nunbal(1)

Maximum values of the 3 phase-to-neutral voltage unbalances V1Nunbal MAX, V2Nunbal MAX, V3Nunbal MAX(1)

Real-time maximum of 3 phase-to-neutral voltage unbalances(1)

Maximum of maximum of 3 phase-to-neutral voltage unbalances(1)

(1) Applies to 4-pole circuit breakers or 3-pole circuit breakers with ENVT wired and configured.

Power

Measurement

MicroLogic X HMI

EPD app

EPC software

FDM128

FDM121

Communication

IFE/EIFE webpages

Real-time active power for each phase P1, P2, P3(1)

Maximum values of active power for each phase P1 MAX, P2 MAX, P3 MAX(1)

Minimum values of active power for each phase P1 MIN, P2 MIN, P3 MIN(1)

Real-time total active power Ptot

Maximum value of total active power Ptot MAX

Minimum value of total active power Ptot MIN

Real-time reactive power for each phase Q1, Q2, Q3(1)

Maximum values of reactive powers for each phase Q1 MAX, Q2 MAX, Q3 MAX(1)

Minimum values of reactive powers for each phase Q1 MIN, Q2 MIN, Q3 MIN(1)

Real-time total reactive power Qtot

Maximum value of total reactive power Qtot MAX

Minimum value of total reactive power Qtot MIN

Real-time apparent power for each phase S1, S2, S3(1)

Maximum values of apparent powers for each phase S1 MAX, S2 MAX, S3 MAX(1)

Minimum values of apparent powers for each phase S1 MIN, S2 MIN, S3 MIN(1)

Real-time total apparent power Stot

Maximum value of total apparent power Stot MAX

Minimum value of total apparent power Stot MIN

(1) Applies to 4-pole circuit breakers or 3-pole circuit breakers with ENVT wired and configured.

Operating Indicators

Measurement

MicroLogic X HMI

EPD app

EPC software

FDM128

FDM121

Communication

IFE/EIFE webpages

Operating quadrant

Phase rotation

Type of load

Power Factor PF and cos φ

Measurement

MicroLogic X HMI

EPD app

EPC software

FDM128

FDM121

Communication

IFE/EIFE webpages

Real-time total power factor PF

Maximum value of the total power factor PF MAX

Minimum value of the total power factor PF MIN

Real-time power factors for each phase PF1, PF2, PF3(1)

Maximum power factor for each phase PF1 MAX, PF2 MAX, PF3 MAX(1)

Minimum power factor for each phase PF1 MIN, PF2 MIN, PF3 MIN(1)

Real-time total cos φ

Maximum value cos φ MAX

Minimum value cos φ MIN

Real-time cos φ for each phase cos φ 1, cos φ 2, cos φ 3(1)

Maximum cos φ for each phase cos φ 1 MAX, cos φ 2 MAX, cos φ 3 MAX(1)

Minimum cos φ for each phase cos φ 1 MIN, cos φ 2 MIN, cos φ 3 MIN(1)

(1) Applies to 4-pole circuit breakers or 3-pole circuit breakers with ENVT wired and configured.

Total Harmonic Distortion Compared to the Fundamental (THD) of Currents

Measurement

MicroLogic X HMI

EPD app

EPC software

FDM128

FDM121

Communication

IFE/EIFE webpages

Real-time total harmonic distortion (THD) of current for each phase THD(I1), THD(I2), THD(I3)

Real-time total harmonic distortion (THD) of neutral current THD(IN)(1)

Maximum value of total harmonic distortion (THD) of neutral current THD(IN) MAX(1)

Minimum value of total harmonic distortion (THD) of neutral current THD(IN) MIN(1)

Real-time average total harmonic distortion (THD) of the 3 phase currents

Maximum value of the average total harmonic distortion (THD) of the 3 phase currents

Minimum value of the average total harmonic distortion (THD) of the 3 phase currents

(1) Applies to 4-pole circuit breakers or 3-pole circuit breakers with ENVT wired and configured.

Total Harmonic Distortion Compared to the Fundamental (THD) of Voltages

Measurement

MicroLogic X HMI

EPD app

EPC software

FDM128

FDM121

Communication

IFE/EIFE webpages

Real-time total harmonic distortion (THD) of phase-to-phase voltage THD(V12), THD(V23), THD(V31)

Real-time total harmonic distortion (THD) of phase-to-neutral voltage THD(V1N), THD(V2N), THD(V3N)(1)

Real-time average total harmonic distortion (THD) of the 3 phase-to-phase voltages

Maximum value of the average total harmonic distortion (THD) of the 3 phase-to-phase voltages

Minimum value of the average total harmonic distortion (THD) of the 3 phase-to-phase voltages

Real-time average total harmonic distortion (THD) of the 3 phase-to-neutral voltages(1)

Maximum value of the average total harmonic distortion (THD) of the 3 phase-to-neutral voltages(1)

Minimum value of the average total harmonic distortion (THD) of the 3 phase-to-neutral voltages(1)

(1) Applies to 4-pole circuit breakers or 3-pole circuit breakers with ENVT wired and configured.

Total Harmonic Distortion Compared to the RMS Value (THD-R) of Currents

Measurement

MicroLogic X HMI

EPD app

EPC software

FDM128

FDM121

Communication

IFE/EIFE webpages

Real-time total harmonic distortion (THD-R) of current for each phase THD-R(I1), THD-R(I2), THD-R(I3)

Real-time total harmonic distortion (THD-R) of neutral current THD-R(IN)(1)

Maximum value of total harmonic distortion (THD-R) of neutral current THD-R(IN) MAX(1)

Minimum value of total harmonic distortion (THD-R) of neutral current THD-R(IN) MIN(1)

Real-time average total harmonic distortion (THD-R) of the 3 phase currents

Maximum value of the average total harmonic distortion (THD-R) of the 3 phase currents

Minimum value of the average total harmonic distortion (THD-R) of the 3 phase currents

(1) Applies to 4-pole circuit breakers or 3-pole circuit breakers with ENVT wired and configured.

Total Harmonic Distortion Compared to the RMS Value (THD-R) of Voltages

Measurement

MicroLogic X HMI

EPD app

EPC software

FDM128

FDM121

Communication

IFE/EIFE webpages

Real-time total harmonic distortion (THD-R) of the phase-to-phase voltage THD-R(V12), THD-R(V23), THD-R(V31)

Real-time total harmonic distortion (THD-R) of the phase-to-neutral voltage THD-R(V1N), THD-R(V2N), THD-R(V3N)(1)

Real-time average total harmonic distortion (THD-R) of the 3 phase-to-phase voltages

Maximum value of the average total harmonic distortion (THD-R) of the 3 phase-to-phase voltages

Minimum value of the average total harmonic distortion (THD-R) of the 3 phase-to-phase voltages

Real-time average total harmonic distortion (THD-R) of the 3 phase-to-neutral voltages(1)

Maximum value of the average total harmonic distortion (THD-R) of the 3 phase-to-neutral voltages(1)

Minimum value of the average total harmonic distortion (THD-R) of the 3 phase-to-neutral voltages(1)

(1) Applies to 4-pole circuit breakers or 3-pole circuit breakers with ENVT wired and configured.

Frequency

Measurement

MicroLogic X HMI

EPD app

EPC software

FDM128

FDM121

Communication

IFE/EIFE webpages

Frequency

Maximum frequency

Minimum frequency

Current Demand and Peak Values

Measurement

MicroLogic X HMI

EPD app

EPC software

FDM128

FDM121

Communication

IFE/EIFE webpages

Phase (I1, I2, I3) current demand values

Phase (I1, I2, I3) peak current demand values

Neutral (IN) current demand value(1)

Neutral (IN) peak current demand value(1)

Average (Iavg) current demand value

Average (Iavg) peak current demand value

(1) Applies to 4-pole circuit breakers or 3-pole circuit breakers with ENVT wired and configured.

Power Demand and Peak Values

Measurement

MicroLogic X HMI

EPD app

EPC software

FDM128

FDM121

Communication

IFE/EIFE webpages

Demand value (P dmd) of the total active power (Ptot)

Peak demand value (P dmd max) of the total active power (Ptot)

Demand value (Q dmd) of the total reactive power (Qtot)

Peak demand value (Q dmd max) of the total reactive power (Qtot)

Demand value (S dmd) of the total apparent power (Stot)

Peak demand value (S dmd max) of the total apparent power (Stot)

Resettable Energy Meters

Measurement

MicroLogic X HMI

EPD app

EPC software

FDM128

FDM121

Communication

IFE/EIFE webpages

Total active energy value Ep

Total active energy values: Epdelivered, and Epreceived

Total reactive energy value Eq

Total reactive energy values: Eqdelivered, and Eqreceived

Total apparent energy value Es

Non-Resettable Energy Meters

Measurement

MicroLogic X HMI

EPD app

EPC software

FDM128

FDM121

Communication

IFE/EIFE webpages

Total active energy value Ep

Total active energy values: Epdelivered, and Epreceived

Total reactive energy value Eq

Total reactive energy values: Eqdelivered, and Eqreceived

Total apparent energy value Es

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.