GEX2563900SWE-00(NORDICS)

Applied Standards

Series PIX switchgear units with vacuum switching devices are:

  • Metal-enclosed; loss of service continuity category accordance
    IEC 62271-200: 2011 LSC 2B-PM

  • Type-tested

  • Optional: tested for internal faults (qualification IAC)

  • Dimensioned for indoor installation.

The PIX switchgear units meet the following standards and regulations:

Designation

IEC/EN-Standard

Switchgear

IEC 62271-200: 2011

IEC 62271-1: 2017

Internal arc classification (IAC)

IEC 62271-200: 2011

Circuit breaker

IEC 62271-100: 2017

Vacuum contactor

IEC 60470

Earthing switch

IEC 62271-102: 2018

Disconnector truck

IEC 62271-102: 2018

Current transformer

IEC 61869-2: 2012

Voltage transformer

IEC 61869-3: 2011

Voltage presence Indicating systems (VPIS)

IEC 62271-206: 2011

Voltage detection indication system (VDIS)

IEC 62271-213: 2021

Protection against accidental contact, foreign bodies and water

IEC 62271-200: 2011

IEC 60529: 2013

Installation

IEC 61936-1

Operation of electrical equipment

EN 50110-1

High-voltage fuse link

IEC 60644: 2009

IEC 60282-1: 2009

Degrees of protection against accidental contact and foreign objects

Degrees of protection against accidental contact and foreign objects according to IEC 60529: 2013

External enclosure of panel

IP3X(1)

Between the compartments of the panel

IP2X

(1) Optional IP4X; other values available on request.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.